Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Class and Description |
---|
ComplexScalarFieldWrapper
This class defines a complex value that is internally
backed up by a field or two expressions.
|
FieldExpression
Represents the Field Expression class.
|
FieldManager
Represents the manager class of the Fields
This manager class gives access to all the fields Field within a part,
as well as the collection of domains FieldDomain . |
FieldWrapper
This class defines a value that is internally backed up by a field.
|
ScalarFieldWrapper
This class defines a scalar value that is internally
backed up by a (optionally scaled) field or an expression.
|
Class and Description |
---|
Field
Represents an Field abstract class.
|
FieldExpression
Represents the Field Expression class.
|
FieldManager
Represents the manager class of the Fields
This manager class gives access to all the fields Field within a part,
as well as the collection of domains FieldDomain . |
FieldReference
Represents an reference field
A Reference Field exposes data inside of an abstract data store. |
FieldTable
Represents the Field Table class.
|
FieldVariable
Represents the Field Variables
A variable is a symbol on whose value a function, polynomial, etc., depends. |
FieldWrapper
This class defines a value that is internally backed up by a field.
|
NameVariable
This class stores the common name and measure for field variables.
|
VectorFieldWrapper
This class defines a vector value that is internally
backed up by a (optionally scaled) field or three expressions.
|
Class and Description |
---|
ComplexScalarFieldWrapper
This class defines a complex value that is internally
backed up by a field or two expressions.
|
DisplayPropertiesBuilder |
DisplayPropertiesBuilder.DepDispTypeEnum
Field Dep Disp Type
|
DisplayPropertiesBuilder.DepDomColorEnum
Field Dep Dom Color
|
DisplayPropertiesBuilder.DepLabelValueEnum
Field Dep Label Value
|
DisplayPropertiesBuilder.DispResolutionEnum
Field Disp Resolution
|
DisplayPropertiesBuilder.IndepDomDispType
Field Indep Dom Disp
|
DisplayPropertiesBuilder.LineFontEnum
Field Line Display Fonts
|
DisplayPropertiesBuilder.LineWidthEnum
Field Line Widths
|
DisplayPropertiesBuilder.TblPointTypeEnum
Field Tbl Point Type
|
DisplayPropertiesBuilder.ValuesEnum
Field Values
|
ExportData
Represents data for field export
To create a new instance of this class, use FieldManager.createExportData() Created in NX6.0.0 |
Field
Represents an Field abstract class.
|
FieldCollection
Represents a collection of Fields
To obtain an instance of this class, refer to FieldManager Created in NX4.0.0 |
FieldDomainCollection
Provides methods for manipulating the field domains
To obtain an instance of this class, refer to FieldManager Created in NX4.0.0 |
FieldEvaluator
Represents a Field Evaluator which can be used to evaluate a
Field . |
FieldEvaluator.InterpolationEnum
Interpolation type
|
FieldEvaluator.InverseDistanceWeightingEnum
Options for IDW (inverse weighted distance) interpolator
|
FieldEvaluator.LinearLogOptionEnum
Log Options for Linear interpolator
|
FieldEvaluator.ValuesOutsideTableInterpolationEnum
Options for outside table values interpolation
|
FieldExpression
Represents the Field Expression class.
|
FieldFormula
Represents the Field Formula class.
|
FieldLink
Represents the Field Link class.
|
FieldLinksTable
Represents the Field LinksTable class.
|
FieldTable
Represents the Field Table class.
|
FieldTable.IdwOptionsData
This class holds the data returned from
FieldTable.getIdwOptions() |
FieldTable.InterpolationEnum
Deprecated.
Deprecated in NX7.5.2. Use
FieldEvaluator.InterpolationEnum instead.
|
FieldTable.LoadFileOption
Load file options
|
FieldVariable
Represents the Field Variables
A variable is a symbol on whose value a function, polynomial, etc., depends. |
FieldVariable.Bounds
Variable Bounds structure
|
FieldVariable.Type
Variable Types
|
FieldVariable.ValueType
Variable value Type
|
FieldWrapper
This class defines a value that is internally backed up by a field.
|
ImportData
Represents data transfer objectst for field import
To create a new instance of this class, use FieldManager.createImportData() Created in NX6.0.0 |
NameVariable
This class stores the common name and measure for field variables.
|
PathObjects
Contains objects that define a lattice path
Not a KF builder; see Fields.FieldManager methods to create a Fields.PathObjects. |
PathObjectsList
Represents a list of objects.
|
ScalarFieldWrapper
This class defines a scalar value that is internally
backed up by a (optionally scaled) field or an expression.
|
SpatialMap
Represents the Field Domain Map
A Spatial Map provides a mapping from a field's independent domain into a new domain space. |
SpatialMap.BoundingBoxMapEnum
Bounding Box Map
|
SpatialMap.ParametricPlaneMapEnum
Parametric Plane Map
|
SpatialMap.SubtypeEnum
Subtype of Spatial Map
|
SpatialMap.SubtypeMappingEnum
Subtype Mapping
|
SpatialMap.TypeEnum
Type of Spatial Map
|
SpatialMapBuilder |
VectorFieldWrapper
This class defines a vector value that is internally
backed up by a (optionally scaled) field or three expressions.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.