public static class FieldEvaluator.InverseDistanceWeightingEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL
Sum of the weighted value of all points, based on the inverse of the distance
|
static int |
_NEAREST_POINTS
Sum of the weighted value of N nearest points (as a fraction of the total number of points), based on the inverse of the distance
|
static int |
_RADIUS
Sum of the weighted value of points within a radius (as a fraction of the bounding box diagonal), based on the inverse of the distance
|
static FieldEvaluator.InverseDistanceWeightingEnum |
ALL
Sum of the weighted value of all points, based on the inverse of the distance
|
static FieldEvaluator.InverseDistanceWeightingEnum |
NEAREST_POINTS
Sum of the weighted value of N nearest points (as a fraction of the total number of points), based on the inverse of the distance
|
static FieldEvaluator.InverseDistanceWeightingEnum |
RADIUS
Sum of the weighted value of points within a radius (as a fraction of the bounding box diagonal), based on the inverse of the distance
|
Modifier and Type | Method and Description |
---|---|
static FieldEvaluator.InverseDistanceWeightingEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FieldEvaluator.InverseDistanceWeightingEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FieldEvaluator.InverseDistanceWeightingEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final FieldEvaluator.InverseDistanceWeightingEnum ALL
public static final FieldEvaluator.InverseDistanceWeightingEnum RADIUS
public static final FieldEvaluator.InverseDistanceWeightingEnum NEAREST_POINTS
public static final int _ALL
public static final int _RADIUS
public static final int _NEAREST_POINTS
public static FieldEvaluator.InverseDistanceWeightingEnum valueOf(int value)
public static FieldEvaluator.InverseDistanceWeightingEnum valueOf(String name)
public static FieldEvaluator.InverseDistanceWeightingEnum[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.