public static class SeatBeltAnchorageBuilder.LTwoLimitType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEGREE45AND80
L2 limit angle area between 45 degree and 80 degree
|
static int |
_DEGREE50AND70
L2 limit angle area between 50 degree and 70 degree
|
static SeatBeltAnchorageBuilder.LTwoLimitType |
DEGREE45AND80
L2 limit angle area between 45 degree and 80 degree
|
static SeatBeltAnchorageBuilder.LTwoLimitType |
DEGREE50AND70
L2 limit angle area between 50 degree and 70 degree
|
Modifier and Type | Method and Description |
---|---|
static SeatBeltAnchorageBuilder.LTwoLimitType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeatBeltAnchorageBuilder.LTwoLimitType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeatBeltAnchorageBuilder.LTwoLimitType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SeatBeltAnchorageBuilder.LTwoLimitType DEGREE45AND80
public static final SeatBeltAnchorageBuilder.LTwoLimitType DEGREE50AND70
public static final int _DEGREE45AND80
public static final int _DEGREE50AND70
public static SeatBeltAnchorageBuilder.LTwoLimitType valueOf(int value)
public static SeatBeltAnchorageBuilder.LTwoLimitType valueOf(String name)
public static SeatBeltAnchorageBuilder.LTwoLimitType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.