public static class SeatBeltAnchorageBuilder.LOneLimitType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEGREE30AND80
L1 limit angle area between 30 degree and 80 degree
|
static int |
_DEGREE50AND70
L1 limit angle area between 50 degree and 70 degree
|
static SeatBeltAnchorageBuilder.LOneLimitType |
DEGREE30AND80
L1 limit angle area between 30 degree and 80 degree
|
static SeatBeltAnchorageBuilder.LOneLimitType |
DEGREE50AND70
L1 limit angle area between 50 degree and 70 degree
|
Modifier and Type | Method and Description |
---|---|
static SeatBeltAnchorageBuilder.LOneLimitType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeatBeltAnchorageBuilder.LOneLimitType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeatBeltAnchorageBuilder.LOneLimitType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SeatBeltAnchorageBuilder.LOneLimitType DEGREE30AND80
public static final SeatBeltAnchorageBuilder.LOneLimitType DEGREE50AND70
public static final int _DEGREE30AND80
public static final int _DEGREE50AND70
public static SeatBeltAnchorageBuilder.LOneLimitType valueOf(int value)
public static SeatBeltAnchorageBuilder.LOneLimitType valueOf(String name)
public static SeatBeltAnchorageBuilder.LOneLimitType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.