public static class SeatBeltAnchorageBuilder.LowerAreaType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NO
hide lower area
|
static int |
_YES
show lower area
|
static SeatBeltAnchorageBuilder.LowerAreaType |
NO
hide lower area
|
static SeatBeltAnchorageBuilder.LowerAreaType |
YES
show lower area
|
Modifier and Type | Method and Description |
---|---|
static SeatBeltAnchorageBuilder.LowerAreaType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeatBeltAnchorageBuilder.LowerAreaType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeatBeltAnchorageBuilder.LowerAreaType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SeatBeltAnchorageBuilder.LowerAreaType YES
public static final SeatBeltAnchorageBuilder.LowerAreaType NO
public static final int _YES
public static final int _NO
public static SeatBeltAnchorageBuilder.LowerAreaType valueOf(int value)
public static SeatBeltAnchorageBuilder.LowerAreaType valueOf(String name)
public static SeatBeltAnchorageBuilder.LowerAreaType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.