Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Class and Description |
---|
AllAroundVision
Represents an all-around vision feature
To create or edit an instance of this class, use AllAroundVisionBuilder Created in NX8.5.0 |
AllAroundVisionBuilder
A
AllAroundVisionBuilder used to create or edit
a vehicle design AllAroundVision feature. |
BaseDataBuilder
Represents a
BaseDataBuilder . |
BaseDataImportExportBuilder
Represents a
BaseDataImportExportBuilder
builder used to import and export expressions from and to a spreadsheet. |
BumperPendulum
Represents a bumper pendulum feature
To create or edit an instance of this class, use BumperPendulumBuilder Created in NX8.5.0 |
BumperPendulumBuilder
Represents a
BumperPendulum builder
To create a new instance of this class, use VehicleDesignCollection.createBumperPendulumBuilder(nxopen.features.vehicledesign.BumperPendulum) Default values. |
CloseRangeVisibility
Represents a close range visibility feature
To create or edit an instance of this class, use CloseRangeVisibilityBuilder Created in NX8.5.0 |
CloseRangeVisibilityBuilder
The builder to create close range visibility feature.
|
CrashBarrier
Represents a crash barrier feature
To create or edit an instance of this class, use CrashBarrierBuilder Created in NX8.5.0 |
CrashBarrierBuilder
Represents a
CrashBarrier builder
to create and edit a vehicle design crash barrier. |
DynamicCurb
Represents a dynamic curb feature
To create or edit an instance of this class, use DynamicCurbBuilder Created in NX8.5.0 |
DynamicCurbBuilder
Represents a
DynamicCurb builder
To create a new instance of this class, use VehicleDesignCollection.createDynamicCurbBuilder(nxopen.features.vehicledesign.DynamicCurb) Default values. |
GroundClearance
Represents a ground clearance feature.
|
GroundClearanceBuilder
Represents a
GroundClearance builder. |
HeadImpact
Represents a head impact feature.
|
HeadImpactAPillar
Represents a head impact a-pillar feature.
|
HeadImpactAPillarBuilder
Represents a
HeadImpactAPillarBuilder . |
HeadImpactBPillar
Represents a head impact b-pillar feature.
|
HeadImpactBPillarBuilder
Represents a
HeadImpactBPillarBuilder . |
HeadImpactBuilder
Represents a
HeadImpactBuilder . |
HeadImpactFrontHeader
Represents a head impact front header feature.
|
HeadImpactFrontHeaderBuilder
Represents a
HeadImpactFrontHeaderBuilder . |
HeadImpactOPillar
Represents a head impact side rail feature.
|
HeadImpactOPillarBuilder
Represents a
HeadImpactOPillarBuilder . |
HeadImpactOtherRail
Represents a head impact additional side rail feature.
|
HeadImpactOtherRailBuilder
Represents a
HeadImpactOtherRailBuilder . |
HeadImpactRearHeader
Represents a head impact rear header feature.
|
HeadImpactRearHeaderBuilder
Represents a
HeadImpactRearHeaderBuilder . |
HeadImpactRPillar
Represents a head impact rear pillar feature.
|
HeadImpactRPillarBuilder
Represents a
HeadImpactRPillarBuilder . |
HeadImpactSideRail
Represents a head impact side rail feature.
|
HeadImpactSideRailBuilder
Represents a
HeadImpactSideRailBuilder . |
HeadImpactUpperRoof
Represents a head impact upper roof feature.
|
HeadImpactUpperRoofBuilder
Represents a
HeadImpactUpperRoofBuilder . |
HoodVisibility
Represents a hood visibility spline feature
To create or edit an instance of this class, use HoodVisibilityBuilder Created in NX6.0.0 |
HoodVisibilityBuilder
Represents a
HoodVisibility builder
To create a new instance of this class, use VehicleDesignCollection.createHoodVisibilityBuilder(nxopen.features.vehicledesign.HoodVisibility) Default values. |
InnerAngle
Represents an inner angle feature
To create or edit an instance of this class, use InnerAngleBuilder Created in NX8.5.0 |
InnerAngleBuilder
Represents a
InnerAngle builder,
used to create or edit inner angle feature. |
Manikin
Represents a manikin automotive feature
To create or edit an instance of this class, use ManikinBuilder Created in NX7.5.0 |
ManikinBuilder
Represents a
Manikin builder
To create a new instance of this class, use VehicleDesignCollection.createManikinBuilder(nxopen.features.vehicledesign.Manikin) Default values. |
MirrorCertification
Represents a mirror certification feature.
|
MirrorCertificationBuilder
A
MirrorCertificationBuilder used to create or edit
a vehicle design MirrorCertification feature. |
OilPan
Represents a oil pan feature
To create or edit an instance of this class, use OilPanBuilder Created in NX8.5.0 |
OilPanBuilder
Represents a
OilPan builder to create and edit a vehicle design oil pan. |
PedestrianProtection
Represents a pedestrian protection feature
To create or edit an instance of this class, use PedestrianProtectionBuilder Created in NX6.0.0 |
PedestrianProtectionBuilder
Represents a
PedestrianProtection builder
To create a new instance of this class, use VehicleDesignCollection.createPedestrianProtectionBuilder(nxopen.features.vehicledesign.PedestrianProtection) Default values. |
ReflectionData
Represents a reflection data feature
To create or edit an instance of this class, use ReflectionDataBuilder Created in NX6.0.0 |
ReflectionDataBuilder
Represents a
ReflectionData builder
To create a new instance of this class, use VehicleDesignCollection.createReflectionDataBuilder(nxopen.features.vehicledesign.ReflectionData) Default values. |
SeatBeltAnchorage
Represents a seat belt anchorage feature
To create or edit an instance of this class, use SeatBeltAnchorageBuilder Created in NX6.0.0 |
SeatBeltAnchorageBuilder
Represents a
Features.VehicleDesign.SeatBeltAnchorage builder
To create a new instance of this class, use VehicleDesignCollection.createSeatBeltAnchorageBuilder(nxopen.features.vehicledesign.SeatBeltAnchorage) Default values. |
Slope
Represents a Slope feature
To create or edit an instance of this class, use SlopeBuilder Created in NX8.5.0 |
SlopeBuilder
The builder to create slope feature.
|
StaticCurb
Represents a static curb feature
To create or edit an instance of this class, use StaticCurbBuilder Created in NX8.5.0 |
StaticCurbBuilder
Represents a
StaticCurb builder
used to create or edit static curb feature
To create a new instance of this class, use VehicleDesignCollection.createStaticCurbBuilder(nxopen.features.vehicledesign.StaticCurb) Default values. |
TireEnvelope
Represents a tire envelope feature
To create or edit an instance of this class, use TireEnvelopeBuilder Created in NX7.5.0 |
TireEnvelopeBuilder
Represents a builder that is used to edit or create a
TireEnvelope . |
VehicleCoordinateSystem
Represents a vehicle coordinate system feature
To create or edit an instance of this class, use VehicleCoordinateSystemBuilder Created in NX7.0.0 |
VehicleCoordinateSystemBuilder
Represents a
VehicleCoordinateSystem builder
To create a new instance of this class, use VehicleDesignCollection.createVehicleCoordinateSystemBuilder(nxopen.features.vehicledesign.VehicleCoordinateSystem) Created in NX7.0.0 |
VisionPlane
Represents a vision plane feature.
|
VisionPlaneBuilder
Represents a
VisionPlane builder used to create or edit a Vision Plane. |
WheelCovering
Represents a wheel covering feature
To create or edit an instance of this class, use WheelCoveringBuilder Created in NX8.5.0 |
WheelCoveringBuilder
Represents a
WheelCovering
feature builder for wheel covering surface section checking. |
WheelFixing
Represents a wheel fixing feature
To create or edit an instance of this class, use WheelFixingBuilder Created in NX8.5.0 |
WheelFixingBuilder
Represents a
WheelFixing builder used to
create or edit a vehicle design wheel fixing. |
WindshieldDatum
Represents a windshield datum feature.
|
WindshieldDatumBuilder
Represents a
WindshieldDatum builder used to create or edit a Windshield Datum. |
Class and Description |
---|
AllAroundVisionBuilder.Types
Used to indicate the type of obstructing geometry to use.
|
AllAroundVisionBuilder.WindowTypes
Used to indicate the type of geometry used to define the window.
|
BaseDataDriverBuilder
Represents a
BaseDataDriverBuilder . |
BaseDataImportExportBuilder.AssignItemNumberData
This class holds the data returned from
BaseDataImportExportBuilder.assignItemNumber() |
BaseDataImportExportBuilder.AssignItemRevisionData
This class holds the data returned from
BaseDataImportExportBuilder.assignItemRevision(java.lang.String) |
BaseDataImportExportBuilder.ExportOptions
This enum represents the option to indicate if the expressions are to be exported to a new item or an existing item in Teamcenter.
|
BaseDataImportExportBuilder.OperateOptions
This enum represents the import or export operate options
|
BaseDataLoadingBuilder
Represents a
BaseDataLoadingBuilder . |
BaseDataLoadingBuilder.LoadingType
This enum represents the vehicle loading types.
|
BaseDataLoadingWheelBuilder
Represents a
BaseDataLoadingWheelBuilder . |
BaseDataLoadingWheelBuilder.DataDefinitionOptions
This enum represents the options to define the wheel position.
|
BaseDataPassengerBuilder
Represents a
BaseDataPassengerBuilder . |
BaseDataPassengerBuilder.SeatDirectionOptions
This enum represents the options to define the passenger's seat direction type.
|
BaseDataWheelBuilder
Represents a
BaseDataWheelBuilder . |
BaseDataWheelBuilder.PositionDefinitionOptions
This enum represents the options to define the wheel position.
|
BumperPendulumBuilder.RequirementsControlType
Represents the requirements control types to define the bumper pendulum.
|
BumperPendulumBuilder.VisualizationType
Represents the visualization types of the output.
|
CloseRangeCameraListItemBuilder
Represents the builder to create camera list item used for close range visibility.
|
CloseRangeCameraListItemBuilder.Types
This enum represents the camera definition options to define the close range visibility.
|
CloseRangeCameraListItemBuilderList
Represents a list of objects.
|
CloseRangeDemoCylinderListItemBuilder
Represents the builder to create demo cylinder list item used for close range visibility.
|
CloseRangeDemoCylinderListItemBuilder.ValidateTypes
This enum represents the simple or detailed checking options to validate demo cylinders visibility.
|
CloseRangeDemoCylinderListItemBuilderList
Represents a list of objects.
|
CloseRangeVisibilityBuilder.EyePointOffsetTypes
This enum represents the eye position offset options.
|
CloseRangeVisibilityBuilder.EyePointTypes
This enum represents the binocular or monocular eye position definition options.
|
CloseRangeVisibilityBuilder.PathPositionTypes
This enum represents the cylinder path position display options.
|
CloseRangeVisibilityBuilder.PositionMethods
This enum represents the cylinder position method options.
|
CloseRangeVisibilityBuilder.PositionPaths
This enum represents the cylinder position path options.
|
CloseRangeVisibilityBuilder.RequirementsControlType
This enum represents the standard or user defined requirement options.
|
CrashBarrierBuilder.CrossPositionType
Represents the cross position types.
|
CrashBarrierBuilder.OverlapSideType
Represents the overlap side types for the front and rear barriers.
|
CrashBarrierBuilder.PositionObjectType
Represents the position object types.
|
CrashBarrierBuilder.RequirementsControlsControlType
Represents the requirements control types to define the crash barrier.
|
CrashBarrierBuilder.ShapeType
Represents the shape types.
|
CrashBarrierBuilder.SideOverlapSideType
Represents the overlap side types for side barrier.
|
CrashBarrierBuilder.SidePositionType
Represents the position types for side barrier.
|
DynamicCurbBuilder.MethodType
Represents the type of inner line to create dynamic curb.
|
DynamicCurbBuilder.PositionType
Represents the dynamic curb positions.
|
DynamicCurbBuilder.RequirementsControlType
Represents the requirements control types to define the dynamic curb.
|
DynamicCurbBuilder.VisualizationType
Represents the visualization types of the output.
|
DynamicCurbBuilder.WheelType
Represents the type of the wheel size option for dynamic curb.
|
GroundClearanceBuilder.PositionType
Represents the ground clearance positions.
|
GroundClearanceBuilder.RequirementControls
This enum represents the standard or user defined requirement options for ground clearance.
|
GroundClearanceBuilder.SectionCurveType
Represents the type of under axle section curve type to create ground clearace.
|
GroundClearanceBuilder.SurfaceLengthType
Represents the type of general surface length to create ground clearace.
|
GroundClearanceBuilder.VisualizationTypes
This enum represents the output definition options.
|
GroundClearanceBuilder.WheelType
Represents the type of the wheel size option for ground clearance.
|
HeadImpactAPillar
Represents a head impact a-pillar feature.
|
HeadImpactAPillarDetailBuilder
Represents a
HeadImpactAPillarDetailBuilder . |
HeadImpactAPillarDetailBuilder.MeasurementMethodType
Represents the measurement methods used to position point 1.
|
HeadImpactAPillarWizardBuilder
Represents a
HeadImpactAPillarWizardBuilder . |
HeadImpactBPillar
Represents a head impact b-pillar feature.
|
HeadImpactBPillarDetailBuilder
Represents a
HeadImpactBPillarDetailBuilder . |
HeadImpactBPillarWizardBuilder
Represents a
HeadImpactBPillarWizardBuilder . |
HeadImpactBuilder
Represents a
HeadImpactBuilder . |
HeadImpactBuilder.CalculationType
Represents the calculation types.
|
HeadImpactBuilder.RequirementsControlType
Represents the requirements control types.
|
HeadImpactFrontHeader
Represents a head impact front header feature.
|
HeadImpactFrontHeaderDetailBuilder
Represents a
HeadImpactFrontHeaderDetailBuilder . |
HeadImpactFrontHeaderWizardBuilder
Represents a
HeadImpactFrontHeaderWizardBuilder . |
HeadImpactOPillar
Represents a head impact side rail feature.
|
HeadImpactOPillarDetailBuilder
Represents a
HeadImpactOPillarDetailBuilder . |
HeadImpactOPillarWizardBuilder
Represents a
HeadImpactOPillarWizardBuilder . |
HeadImpactOtherRail
Represents a head impact additional side rail feature.
|
HeadImpactOtherRailDetailBuilder
Represents a
HeadImpactOtherRailDetailBuilder . |
HeadImpactOtherRailWizardBuilder
Represents a
HeadImpactOtherRailWizardBuilder . |
HeadImpactRearHeader
Represents a head impact rear header feature.
|
HeadImpactRearHeaderDetailBuilder
Represents a
HeadImpactRearHeaderDetailBuilder . |
HeadImpactRearHeaderWizardBuilder
Represents a
HeadImpactRearHeaderWizardBuilder . |
HeadImpactRPillar
Represents a head impact rear pillar feature.
|
HeadImpactRPillarDetailBuilder
Represents a
HeadImpactRPillarDetailBuilder . |
HeadImpactRPillarWizardBuilder
Represents a
HeadImpactRPillarWizardBuilder . |
HeadImpactSideRail
Represents a head impact side rail feature.
|
HeadImpactSideRailDetailBuilder
Represents a
HeadImpactSideRailDetailBuilder . |
HeadImpactSideRailWizardBuilder
Represents a
HeadImpactSideRailWizardBuilder . |
HeadImpactUpperRoof
Represents a head impact upper roof feature.
|
HeadImpactUpperRoofDetailBuilder
Represents a
HeadImpactUpperRoofDetailBuilder . |
HeadImpactUpperRoofWizardBuilder
Represents a
HeadImpactUpperRoofWizardBuilder . |
InnerAngleBuilder.CalculationMethodType
Represents the calculation method types to calculate inner angle output.
|
InnerAngleBuilder.RequirementsControlType
Represents the requirements control types to define the inner angle.
|
InnerAngleBuilder.VisualizationType
Represents the visualization types of the output.
|
InnerAngleBuilder.WheelSizeType
Represents the wheel size types to calculate inner angle output.
|
ManikinBuilder.ClassificationType
the vehicle classification type
|
ManikinBuilder.PositionType
the vehicle seat position type
|
ManikinBuilder.SAEPercentileType
the vehicle percentile type
|
ManikinBuilder.StandardType
the vehicle standard type
|
MirrorCertificationBuilder.DriverSideStandardsType
Used to indicate the standard for the driver mirror.
|
MirrorCertificationBuilder.EyeFromOptionType
Used to indicate what part the eye is from.
|
MirrorCertificationBuilder.EyellipsePercentileType
Used to indicate the eyellipse percentile that is used in mirror certification.
|
MirrorCertificationBuilder.EyeMethodType
Used to indicate the method to calculate the eye location based on the distance from the eyellipse to the mirror pivot.
|
MirrorCertificationBuilder.EyePointMethodType
Used to indicate the method to define the eye point.
|
MirrorCertificationBuilder.InsideStandardsType
Used to indicate the standard for the inside mirror.
|
MirrorCertificationBuilder.InstructionFieldPositionType
Used to indicate the postion where the instruction field will be.
|
MirrorCertificationBuilder.InstructionFieldsType
Used to indicate the shape type of the instruction field.
|
MirrorCertificationBuilder.LocationType
Used to indicate the mirror location.
|
MirrorCertificationBuilder.MirrorOrientationType
Used to indicate the method to rotate mirror.
|
MirrorCertificationBuilder.MirrorSurfaceType
Used to indicate the mirror surface type.
|
MirrorCertificationBuilder.PassengerSideStandardsType
Used to indicate the standard for the passenger mirror.
|
MirrorCertificationBuilder.ShowVisionConeType
Used to indicate what vision cone will be shown.
|
OilPanBuilder.PositionType
Represents the oil pan positions.
|
OilPanBuilder.RequirementsControlType
Represents the requirements control types to define the oil pan.
|
OilPanBuilder.VisualizationType
Represents the visualization types of the output.
|
PedestrianProtectionBuilder.Font
Settings for font to create the various output with
|
PedestrianProtectionBuilder.StandardType
Settings for the type of pedestrian protection standard to use in the study
|
PedestrianProtectionBuilder.TransformMethods
Settings for the transform method of pedestrian protection active hood system
|
PedestrianProtectionBuilder.Types
Settings for the type of pedestrian protection impact study
|
PedestrianProtectionBuilder.Wad
Settings for the start, end and boundary wrap around distance line to create
|
PedestrianProtectionBuilder.Width
Settings for width to create the various output with
|
PendulumPlacementBuilder
This builder allows you to define the pendulum placement information for bumper pendulum features in vehicle design.
|
PendulumPlacementBuilder.LocationType
This enum represents the pendulum placement location options.
|
PendulumPlacementBuilder.PendulumProfileType
This enum represents the pendulum placement profile options.
|
PendulumPlacementBuilder.PositionMethodType
This enum represents the pendulum placement method options.
|
PendulumPlacementBuilder.SideType
This enum represents the pendulum placement side options.
|
ReflectionDataBuilder.ResolutionType
the resolution type
|
SeatBeltAnchorageBuilder.AnchorageLocationTypes
the seat belt anchorage location type
|
SeatBeltAnchorageBuilder.ATLType
the show ATL type
|
SeatBeltAnchorageBuilder.LOneLimitType
the lone limit type
|
SeatBeltAnchorageBuilder.LowerAreaType
the lower area type
|
SeatBeltAnchorageBuilder.LowerLimitType
the lower limit type
|
SeatBeltAnchorageBuilder.LTwoLimitType
the ltwo limit type
|
SeatBeltAnchorageBuilder.RoutingTypes
the seat belt routing type
|
SeatBeltAnchorageBuilder.SeatPositionTypes
the seat position type
|
SeatBeltAnchorageBuilder.SeatTypes
the seat type
|
SeatBeltAnchorageBuilder.StandardTypes
the standard type
|
SeatBeltAnchorageBuilder.UpperAreaType
the upper area type
|
SlopeBuilder.PositionType
Represents the slope positions.
|
SlopeBuilder.RequirementsControlType
Represents the requirements control types to define the slope.
|
SlopeBuilder.VisualizationType
Represents the visualization types of the output.
|
SlopeBuilder.WheelSizeType
Represents the wheel size types to calculate slope output.
|
StaticCurbBuilder.PositionType
Represents the static curb positions.
|
StaticCurbBuilder.RequirementsControlType
Represents the requirements control types to define the static curb.
|
StaticCurbBuilder.VisualizationType
Represents the visualization types of the output.
|
TireEnvelopeBuilder.DriverGraphOption
Settings to indicate the driver definition to use with the MacPherson Strut suspension template.
|
TireEnvelopeBuilder.EnvelopeOffsetMethod
Settings to indicate how the offset will be defined.
|
TireEnvelopeBuilder.MotionMethod
Settings to indicate how the suspension system motion will be defined.
|
TireEnvelopeBuilder.SpindleFileLocationOption
Settings to indicate the location to select the spindle file.
|
TireEnvelopeBuilder.SuspensionTemplateType
Settings to indicate the defined suspension template to use.
|
TireEnvelopeBuilder.TireDefinitionOption
Settings to indicate how the tire profile will be defined.
|
VehicleCoordinateSystemBuilder.Types
Vehicle Coordinate System type
|
VisionPlaneBuilder.CustomVisionAngle
Represents the vision angle type to define the Vision Plane.
|
VisionPlaneBuilder.EnumEyeType
Represents the eye definition type to define the Vision Plane.
|
WheelCoveringBuilder.PositionType
Represents the wheel covering positions.
|
WheelCoveringBuilder.RequirementsControlType
Represents the requirements control types to define the wheel covering.
|
WheelCoveringBuilder.SurfacePlaneType
Represents the type of the surface plane.
|
WheelCoveringBuilder.SurfaceSectionType
Represents the type of the surface section.
|
WheelFixingBuilder.ObjectPositionType
Represents the object position used to indicate if the wheel fixing is positioned at the theoretically
widest dimension of the wheel (diameter) or exactly at the wheel geometry of the base data.
|
WheelFixingBuilder.PositionType
Represents the wheel fixing positions.
|
WheelFixingBuilder.RequirementsControlType
Represents the requirements control types to define the wheel fixing.
|
WheelFixingBuilder.ShapeType
Represents the shape used to indicate if the wheel fixing is a block or a circle segment.
|
WheelFixingBuilder.WheelSizeType
Represents the wheel size used to indicate if the wheel fixing is based on static radius or the diameter of the wheels.
|
WindshieldDatumBuilder.CustomVisionAngle
Represents the vision angle type to define the Windshield Datum.
|
WindshieldDatumBuilder.EnumEyeType
Represents the eye definition type to define the Windshield Datum.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.