public static class BaseDataLoadingBuilder.LoadingType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_STANDARD
Standard - Defined in the registration file, user can not delete it.
|
static int |
_USER_DEFINED
User-Defined - user can add or delete it.
|
static BaseDataLoadingBuilder.LoadingType |
STANDARD
Standard - Defined in the registration file, user can not delete it.
|
static BaseDataLoadingBuilder.LoadingType |
USER_DEFINED
User-Defined - user can add or delete it.
|
Modifier and Type | Method and Description |
---|---|
static BaseDataLoadingBuilder.LoadingType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BaseDataLoadingBuilder.LoadingType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BaseDataLoadingBuilder.LoadingType[] |
values()
Returns an array that contains the values for this enum.
|
public static final BaseDataLoadingBuilder.LoadingType STANDARD
public static final BaseDataLoadingBuilder.LoadingType USER_DEFINED
public static final int _STANDARD
public static final int _USER_DEFINED
public static BaseDataLoadingBuilder.LoadingType valueOf(int value)
public static BaseDataLoadingBuilder.LoadingType valueOf(String name)
public static BaseDataLoadingBuilder.LoadingType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.