public static class TireEnvelopeBuilder.EnvelopeOffsetMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CUSTOMER_DEFINED_DATA
Use the data that the user defines.
|
static int |
_FIXED_SECTIONS
Use the values in the fixed sections.
|
static int |
_FROM_OFFSET_FILE
From the offset file.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
CUSTOMER_DEFINED_DATA
Use the data that the user defines.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
FIXED_SECTIONS
Use the values in the fixed sections.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
FROM_OFFSET_FILE
From the offset file.
|
Modifier and Type | Method and Description |
---|---|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final TireEnvelopeBuilder.EnvelopeOffsetMethod FIXED_SECTIONS
public static final TireEnvelopeBuilder.EnvelopeOffsetMethod CUSTOMER_DEFINED_DATA
public static final TireEnvelopeBuilder.EnvelopeOffsetMethod FROM_OFFSET_FILE
public static final int _FIXED_SECTIONS
public static final int _CUSTOMER_DEFINED_DATA
public static final int _FROM_OFFSET_FILE
public static TireEnvelopeBuilder.EnvelopeOffsetMethod valueOf(int value)
public static TireEnvelopeBuilder.EnvelopeOffsetMethod valueOf(String name)
public static TireEnvelopeBuilder.EnvelopeOffsetMethod[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.