WedmOperationBuilder Class¶
-
class
NXOpen.CAM.
WedmOperationBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a WedmOperation Builder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateWedmOperationBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ApiExitName | Returns or sets the api exit name |
BackburnDistanceBuilder | Returns the backburn_distance builder |
BackburnFlag | Returns or sets the Rough and Backburn Flag |
BackburnPasses | Returns or sets the Backburn Passes |
ChannelName | Returns or sets the channel’s name |
ConvexCorner | Returns or sets the convex_corner |
CornerMaximumAngleBuilder | Returns the corner_maximum_angle builder |
CornerMinimumAngleBuilder | Returns the corner_minimum_angle builder |
CornerRadiusBuilder | Returns the corner_radius builder |
CustomBoundaryDataList | Returns the custom boundary data list |
CutParameters | Returns the cut parameter object |
CutPattern | Returns the cut pattern |
CutoffDistanceBuilder | Returns the cutoff_distance builder |
CutoffFlag | Returns or sets the Cutoff Flag |
CutoffFlagBuilder | Returns the cutoff_flag builder |
CutoffStockBuilder | Returns the cutoff_stock builder |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FinishPassesBuilder | Returns the finish_passes builder |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
LayoutCiBuilder | Returns the Save Layer/Layout builder |
LeadInCircleAngleBuilder | Returns the lead_in_circle_angle_builder |
LeadInPointBuilder | Returns the lead_in_point Builder |
LeadInRadiusBuilder | Returns the lead_in_radius_builder |
LeadOutCircleAngleBuilder | Returns the lead_out_circle_angle_builder |
LeadOutPointBuilder | Returns the lead_out_point Builder |
LeadOutRadiusBuilder | Returns the lead_out_radius_builder |
LoopRadius | Returns the loop radius |
MaximumLoopAngle | Returns the maximum loop angle |
MinimumLoopAngle | Returns the minimum loop angle |
MotionOutputBuilder | Returns the motion output builder |
NcmWedmBuilder | Returns the non-cutting builder |
NocoreStockBuilder | Returns the nocore_stock builder |
Notes | Returns the notes builder |
NumTabs | Returns or sets the Tab Points |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RegionMethod | Returns or sets the Tab Points Region Method |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
RetractPointBuilder | Returns the retract_point Builder |
RoughPassesBuilder | Returns the rough_passes builder |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SmoothLeadInDistanceBuilder | Returns the smooth_lead_in_distance builder |
SmoothLeadInOption | Returns or sets the Smooth Leadin Flag |
SmoothLeadOutDistanceBuilder | Returns the smooth_lead_out_distance builder |
SmoothLeadOutOption | Returns or sets the Smooth Leadout Flag |
Smoothing | Returns or sets the smoothing |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
StopPointDistanceBuilder | Returns the stop_point_distance builder |
StopPointFlag | Returns or sets the Stop Point Flag |
StopPointType | Returns or sets the Stop Point Type |
Tag | Returns the Tag for this object. |
ThreadHolePointBuilder | Returns the thread_hole_point Builder |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
WedmArcOutputTypeCiBuilder | Returns the wedm arc output type Builder |
WedmStatusControlCiBuilder | Returns the wedm status control ci Builder |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExecuteApiExit | Execute api exit |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetInPathEventSetData | Returns the in path event data @return the InPathEventSetData builder |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WedmOperationBuilderBackburnPassesTypes Enumeration | the types available for wedm backburn passes |
WedmOperationBuilderConvexCornerTypes Enumeration | the types available for convex corner control |
WedmOperationBuilderCornerSmoothingType Enumeration | the types available for corner smoothing |
WedmOperationBuilderInPathUdeSetTypes Enumeration | Represents the in path ude set type |
WedmOperationBuilderSmoothLeadInTypes Enumeration | the types available for smooth_lead_in |
WedmOperationBuilderSmoothLeadOutTypes Enumeration | the types available for smooth_lead_out_types |
WedmOperationBuilderStopPointFlagTypes Enumeration | the types available for wedm stop point |
WedmOperationBuilderStopPointTypes Enumeration | the types available for wedm stop point |
Property Detail¶
ApiExitName¶
-
WedmOperationBuilder.
ApiExitName
¶ Returns or sets the api exit name
-------------------------------------
Getter Method
Signature
ApiExitName()
Returns: the api exit name Return type: str New in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ApiExitName(exitName)
Parameters: exitName (str) – the api exit name New in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
BackburnDistanceBuilder¶
-
WedmOperationBuilder.
BackburnDistanceBuilder
¶ Returns the backburn_distance builder
-------------------------------------
Getter Method
Signature
BackburnDistanceBuilder()
Returns: the backburn_distance Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
BackburnFlag¶
-
WedmOperationBuilder.
BackburnFlag
¶ Returns or sets the Rough and Backburn Flag
-------------------------------------
Getter Method
Signature
BackburnFlag()
Returns: the Backburn Flag Return type: int New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
BackburnFlag(backburnFlag)
Parameters: backburnFlag (int) – the Backburn Flag New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
BackburnPasses¶
-
WedmOperationBuilder.
BackburnPasses
¶ Returns or sets the Backburn Passes
-------------------------------------
Getter Method
Signature
BackburnPasses()
Returns: the Backburn Passes Return type: NXOpen.CAM.WedmOperationBuilderBackburnPassesTypes
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
BackburnPasses(backburnPasses)
Parameters: backburnPasses ( NXOpen.CAM.WedmOperationBuilderBackburnPassesTypes
) – the Backburn PassesNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ConvexCorner¶
-
WedmOperationBuilder.
ConvexCorner
¶ Returns or sets the convex_corner
-------------------------------------
Getter Method
Signature
ConvexCorner()
Returns: the convex_corner Return type: NXOpen.CAM.WedmOperationBuilderConvexCornerTypes
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
ConvexCorner(convexCorner)
Parameters: convexCorner ( NXOpen.CAM.WedmOperationBuilderConvexCornerTypes
) – the cutcom_regNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CornerMaximumAngleBuilder¶
-
WedmOperationBuilder.
CornerMaximumAngleBuilder
¶ Returns the corner_maximum_angle builder
-------------------------------------
Getter Method
Signature
CornerMaximumAngleBuilder()
Returns: the corner_maximum_angle Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CornerMinimumAngleBuilder¶
-
WedmOperationBuilder.
CornerMinimumAngleBuilder
¶ Returns the corner_minimum_angle builder
-------------------------------------
Getter Method
Signature
CornerMinimumAngleBuilder()
Returns: the corner_minimum_angle Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CornerRadiusBuilder¶
-
WedmOperationBuilder.
CornerRadiusBuilder
¶ Returns the corner_radius builder
-------------------------------------
Getter Method
Signature
CornerRadiusBuilder()
Returns: the corner_radius Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CustomBoundaryDataList¶
-
WedmOperationBuilder.
CustomBoundaryDataList
¶ Returns the custom boundary data list
-------------------------------------
Getter Method
Signature
CustomBoundaryDataList()
Returns: the custom boundary data list Return type: NXOpen.CAM.WedmCustomBoundaryDataBuilderList
New in version NX8.0.1.
License requirements: cam_base (“CAM BASE”)
CutParameters¶
-
WedmOperationBuilder.
CutParameters
¶ Returns the cut parameter object
-------------------------------------
Getter Method
Signature
CutParameters()
Returns: Return type: NXOpen.CAM.WedmCutParameters
New in version NX7.5.0.
License requirements: None.
CutPattern¶
-
WedmOperationBuilder.
CutPattern
¶ Returns the cut pattern
-------------------------------------
Getter Method
Signature
CutPattern()
Returns: The cut pattern Builder Return type: NXOpen.CAM.CutPatternBuilder
New in version NX7.5.0.
License requirements: None.
CutoffDistanceBuilder¶
-
WedmOperationBuilder.
CutoffDistanceBuilder
¶ Returns the cutoff_distance builder
-------------------------------------
Getter Method
Signature
CutoffDistanceBuilder()
Returns: the cutoff_distance Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutoffFlag¶
-
WedmOperationBuilder.
CutoffFlag
¶ Returns or sets the Cutoff Flag
-------------------------------------
Getter Method
Signature
CutoffFlag()
Returns: the Cutoff Flag Return type: int New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
CutoffFlag(cutoffFlag)
Parameters: cutoffFlag (int) – the Cutoff Flag New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutoffFlagBuilder¶
-
WedmOperationBuilder.
CutoffFlagBuilder
¶ Returns the cutoff_flag builder
-------------------------------------
Getter Method
Signature
CutoffFlagBuilder()
Returns: the cutoff_flag Builder Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutoffStockBuilder¶
-
WedmOperationBuilder.
CutoffStockBuilder
¶ Returns the cutoff_stock builder
-------------------------------------
Getter Method
Signature
CutoffStockBuilder()
Returns: the cutoff_stock Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
FinishPassesBuilder¶
-
WedmOperationBuilder.
FinishPassesBuilder
¶ Returns the finish_passes builder
-------------------------------------
Getter Method
Signature
FinishPassesBuilder()
Returns: the finish_passes Builder Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LayoutCiBuilder¶
-
WedmOperationBuilder.
LayoutCiBuilder
¶ Returns the Save Layer/Layout builder
-------------------------------------
Getter Method
Signature
LayoutCiBuilder()
Returns: the save layer/layout builder Return type: NXOpen.CAM.LayoutCiBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LeadInCircleAngleBuilder¶
-
WedmOperationBuilder.
LeadInCircleAngleBuilder
¶ Returns the lead_in_circle_angle_builder
-------------------------------------
Getter Method
Signature
LeadInCircleAngleBuilder()
Returns: the lead_in_circle_angle_builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LeadInPointBuilder¶
-
WedmOperationBuilder.
LeadInPointBuilder
¶ Returns the lead_in_point Builder
-------------------------------------
Getter Method
Signature
LeadInPointBuilder()
Returns: the lead_in_point Builder Return type: NXOpen.CAM.WedmPointDefinitionBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LeadInRadiusBuilder¶
-
WedmOperationBuilder.
LeadInRadiusBuilder
¶ Returns the lead_in_radius_builder
-------------------------------------
Getter Method
Signature
LeadInRadiusBuilder()
Returns: the lead_in_radius_builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LeadOutCircleAngleBuilder¶
-
WedmOperationBuilder.
LeadOutCircleAngleBuilder
¶ Returns the lead_out_circle_angle_builder
-------------------------------------
Getter Method
Signature
LeadOutCircleAngleBuilder()
Returns: the lead_out_circle_angle_builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LeadOutPointBuilder¶
-
WedmOperationBuilder.
LeadOutPointBuilder
¶ Returns the lead_out_point Builder
-------------------------------------
Getter Method
Signature
LeadOutPointBuilder()
Returns: the retract_point Builder Return type: NXOpen.CAM.WedmPointDefinitionBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LeadOutRadiusBuilder¶
-
WedmOperationBuilder.
LeadOutRadiusBuilder
¶ Returns the lead_out_radius_builder
-------------------------------------
Getter Method
Signature
LeadOutRadiusBuilder()
Returns: the lead_out_radius_builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LoopRadius¶
-
WedmOperationBuilder.
LoopRadius
¶ Returns the loop radius
-------------------------------------
Getter Method
Signature
LoopRadius()
Returns: the loop radius Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
MaximumLoopAngle¶
-
WedmOperationBuilder.
MaximumLoopAngle
¶ Returns the maximum loop angle
-------------------------------------
Getter Method
Signature
MaximumLoopAngle()
Returns: the maximum loop angle Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
MinimumLoopAngle¶
-
WedmOperationBuilder.
MinimumLoopAngle
¶ Returns the minimum loop angle
-------------------------------------
Getter Method
Signature
MinimumLoopAngle()
Returns: the minimum loop angle Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
NcmWedmBuilder¶
-
WedmOperationBuilder.
NcmWedmBuilder
¶ Returns the non-cutting builder
-------------------------------------
Getter Method
Signature
NcmWedmBuilder()
Returns: the non-cutting builder Return type: NXOpen.CAM.NcmWedmBuilder
New in version NX7.5.0.
License requirements: None.
NocoreStockBuilder¶
-
WedmOperationBuilder.
NocoreStockBuilder
¶ Returns the nocore_stock builder
-------------------------------------
Getter Method
Signature
NocoreStockBuilder()
Returns: the nocore_stock Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
NumTabs¶
-
WedmOperationBuilder.
NumTabs
¶ Returns or sets the Tab Points
-------------------------------------
Getter Method
Signature
NumTabs()
Returns: the Num Tabs Return type: int New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
NumTabs(numTabs)
Parameters: numTabs (int) – the Num Tabs New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
RegionMethod¶
-
WedmOperationBuilder.
RegionMethod
¶ Returns or sets the Tab Points Region Method
-------------------------------------
Getter Method
Signature
RegionMethod()
Returns: the Tab Points Region Method Return type: int New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
RegionMethod(regionMethod)
Parameters: regionMethod (int) – the Tab Points Region Method New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
RetractPointBuilder¶
-
WedmOperationBuilder.
RetractPointBuilder
¶ Returns the retract_point Builder
-------------------------------------
Getter Method
Signature
RetractPointBuilder()
Returns: the retract_point Builder Return type: NXOpen.CAM.WedmPointDefinitionBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
RoughPassesBuilder¶
-
WedmOperationBuilder.
RoughPassesBuilder
¶ Returns the rough_passes builder
-------------------------------------
Getter Method
Signature
RoughPassesBuilder()
Returns: the rough_passes Builder Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SmoothLeadInDistanceBuilder¶
-
WedmOperationBuilder.
SmoothLeadInDistanceBuilder
¶ Returns the smooth_lead_in_distance builder
-------------------------------------
Getter Method
Signature
SmoothLeadInDistanceBuilder()
Returns: the smooth_lead_in_distance Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SmoothLeadInOption¶
-
WedmOperationBuilder.
SmoothLeadInOption
¶ Returns or sets the Smooth Leadin Flag
-------------------------------------
Getter Method
Signature
SmoothLeadInOption()
Returns: the Smooth Leadin Flag Return type: NXOpen.CAM.WedmOperationBuilderSmoothLeadInTypes
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
SmoothLeadInOption(leadInFlag)
Parameters: leadInFlag ( NXOpen.CAM.WedmOperationBuilderSmoothLeadInTypes
) – the Smooth Leadin FlagNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SmoothLeadOutDistanceBuilder¶
-
WedmOperationBuilder.
SmoothLeadOutDistanceBuilder
¶ Returns the smooth_lead_out_distance builder
-------------------------------------
Getter Method
Signature
SmoothLeadOutDistanceBuilder()
Returns: the smooth_lead_out_distance Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SmoothLeadOutOption¶
-
WedmOperationBuilder.
SmoothLeadOutOption
¶ Returns or sets the Smooth Leadout Flag
-------------------------------------
Getter Method
Signature
SmoothLeadOutOption()
Returns: the Smooth Leadout Flag Return type: NXOpen.CAM.WedmOperationBuilderSmoothLeadOutTypes
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
SmoothLeadOutOption(leadOutOption)
Parameters: leadOutOption ( NXOpen.CAM.WedmOperationBuilderSmoothLeadOutTypes
) – the Smooth Leadout FlagNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Smoothing¶
-
WedmOperationBuilder.
Smoothing
¶ Returns or sets the smoothing
-------------------------------------
Getter Method
Signature
Smoothing()
Returns: the smoothing Return type: NXOpen.CAM.WedmOperationBuilderCornerSmoothingType
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Smoothing(smoothing)
Parameters: smoothing ( NXOpen.CAM.WedmOperationBuilderCornerSmoothingType
) – the smoothingNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
StopPointDistanceBuilder¶
-
WedmOperationBuilder.
StopPointDistanceBuilder
¶ Returns the stop_point_distance builder
-------------------------------------
Getter Method
Signature
StopPointDistanceBuilder()
Returns: the stop_point_distance Builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
StopPointFlag¶
-
WedmOperationBuilder.
StopPointFlag
¶ Returns or sets the Stop Point Flag
-------------------------------------
Getter Method
Signature
StopPointFlag()
Returns: the Stop Point Flag Return type: NXOpen.CAM.WedmOperationBuilderStopPointFlagTypes
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
StopPointFlag(stopPointFlag)
Parameters: stopPointFlag ( NXOpen.CAM.WedmOperationBuilderStopPointFlagTypes
) – the Stop Point FlagNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
StopPointType¶
-
WedmOperationBuilder.
StopPointType
¶ Returns or sets the Stop Point Type
-------------------------------------
Getter Method
Signature
StopPointType()
Returns: the Stop Point Type Return type: NXOpen.CAM.WedmOperationBuilderStopPointTypes
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
StopPointType(stopPointType)
Parameters: stopPointType ( NXOpen.CAM.WedmOperationBuilderStopPointTypes
) – the Stop Point TypeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ThreadHolePointBuilder¶
-
WedmOperationBuilder.
ThreadHolePointBuilder
¶ Returns the thread_hole_point Builder
-------------------------------------
Getter Method
Signature
ThreadHolePointBuilder()
Returns: the thread_hole_point Builder Return type: NXOpen.CAM.WedmPointDefinitionBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
WedmArcOutputTypeCiBuilder¶
-
WedmOperationBuilder.
WedmArcOutputTypeCiBuilder
¶ Returns the wedm arc output type Builder
-------------------------------------
Getter Method
Signature
WedmArcOutputTypeCiBuilder()
Returns: the wedm_arc_output_type Builder Return type: NXOpen.CAM.WedmArcOutputTypeCiBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
WedmStatusControlCiBuilder¶
-
WedmOperationBuilder.
WedmStatusControlCiBuilder
¶ Returns the wedm status control ci Builder
-------------------------------------
Getter Method
Signature
WedmStatusControlCiBuilder()
Returns: the wedm_status_control_ci Builder Return type: NXOpen.CAM.WedmStatusControlCiBuilder
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
ExecuteApiExit¶
-
WedmOperationBuilder.
ExecuteApiExit
¶ Execute api exit
Signature
ExecuteApiExit()
New in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
GetInPathEventSetData¶
-
WedmOperationBuilder.
GetInPathEventSetData
¶ Returns the in path event data
Signature
GetInPathEventSetData(passNumber, inPathEventType)
Parameters: - passNumber (int) – the pass number
- inPathEventType (
NXOpen.CAM.WedmOperationBuilderInPathUdeSetTypes
) – in path ude set type
Returns: the InPathEventSetData builder
Return type: New in version NX7.5.0.
License requirements: None.
Validate¶
-
WedmOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.