InPathEventSetData Class¶
-
class
NXOpen.CAM.
InPathEventSetData
¶ Bases:
NXOpen.TaggedObject
Represents in path event
This is a sub-builder class and cannot be directly instantiated
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
UdeSet | Returns the ude set |
UdeSetStatus | Returns or sets the ude set status |
Methods¶
Property Detail¶
UdeSet¶
-
InPathEventSetData.
UdeSet
¶ Returns the ude set
-------------------------------------
Getter Method
Signature
UdeSet()
Returns: the ude set Return type: NXOpen.CAM.UdeSet
New in version NX7.5.0.
License requirements: None.
UdeSetStatus¶
-
InPathEventSetData.
UdeSetStatus
¶ Returns or sets the ude set status
-------------------------------------
Getter Method
Signature
UdeSetStatus()
Returns: the ude set status Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UdeSetStatus(status)
Parameters: status (bool) – the ude set status New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)