WedmStatusControlCiBuilder Class

class NXOpen.CAM.WedmStatusControlCiBuilder

Bases: NXOpen.TaggedObject

Represents a WedmStatusControlCiBuilder

New in version NX7.5.0.

Properties

Property Description
StatusControl Returns or sets the Wedm Status Control Type
Tag Returns the Tag for this object.

Methods

Enumerations

WedmStatusControlCiBuilderStatusTypes Enumeration Available types for status control

Property Detail

StatusControl

WedmStatusControlCiBuilder.StatusControl

Returns or sets the Wedm Status Control Type

-------------------------------------

Getter Method

Signature StatusControl()

Returns:the wedm status control type
Return type:NXOpen.CAM.WedmStatusControlCiBuilderStatusTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StatusControl(statusType)

Parameters:statusType (NXOpen.CAM.WedmStatusControlCiBuilderStatusTypes) – the wedm status control type

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)