WedmArcOutputTypeCiBuilder Class

class NXOpen.CAM.WedmArcOutputTypeCiBuilder

Bases: NXOpen.TaggedObject

Represents a WedmArcOutputTypeCiBuilder

New in version NX7.5.0.

Properties

Property Description
OutputType Returns or sets the Motion Output Type
Tag Returns the Tag for this object.

Methods

Enumerations

WedmArcOutputTypeCiBuilderOutputTypes Enumeration Available types for output

Property Detail

OutputType

WedmArcOutputTypeCiBuilder.OutputType

Returns or sets the Motion Output Type

-------------------------------------

Getter Method

Signature OutputType()

Returns:the motion output type
Return type:NXOpen.CAM.WedmArcOutputTypeCiBuilderOutputTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputType(outputType)

Parameters:outputType (NXOpen.CAM.WedmArcOutputTypeCiBuilderOutputTypes) – the motion output type

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)