WedmArcOutputTypeCiBuilderOutputTypes Enumeration

NXOpen.CAM.WedmArcOutputTypeCiBuilder.OutputTypes is an alias for NXOpen.CAM.WedmArcOutputTypeCiBuilderOutputTypes

class NXOpen.CAM.WedmArcOutputTypeCiBuilderOutputTypes

Bases: object

Available types for output

Enum Members

Enum Member Enum Member Description
LinearOnly
linear only
CirPerpToTaxis
cir perp to taxis
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.