WedmOperationBuilderConvexCornerTypes Enumeration

NXOpen.CAM.WedmOperationBuilder.ConvexCornerTypes is an alias for NXOpen.CAM.WedmOperationBuilderConvexCornerTypes

class NXOpen.CAM.WedmOperationBuilderConvexCornerTypes

Bases: object

the types available for convex corner control

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
RollAround
roll around
Loops
loop
ExtendAndTrim
extend tangents
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.