WedmOperationBuilderInPathUdeSetTypes Enumeration

NXOpen.CAM.WedmOperationBuilder.InPathUdeSetTypes is an alias for NXOpen.CAM.WedmOperationBuilderInPathUdeSetTypes

class NXOpen.CAM.WedmOperationBuilderInPathUdeSetTypes

Bases: object

Represents the in path ude set type

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Start
in path ude set at start
End
in path ude set at end
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.