LayoutCiBuilder Class¶
-
class
NXOpen.CAM.
LayoutCiBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a layout ci Builder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
LayoutName | Returns or sets the layer name value |
LayoutSaveSettings | Returns or sets the save layer settings toggle value |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
SaveLayout | Method to save the layer layout. |
Property Detail¶
LayoutName¶
-
LayoutCiBuilder.
LayoutName
¶ Returns or sets the layer name value
-------------------------------------
Getter Method
Signature
LayoutName()
Returns: the current string value Return type: str New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
LayoutName(stringValue)
Parameters: stringValue (str) – the new string value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
LayoutSaveSettings¶
-
LayoutCiBuilder.
LayoutSaveSettings
¶ Returns or sets the save layer settings toggle value
-------------------------------------
Getter Method
Signature
LayoutSaveSettings()
Returns: the current toggle value Return type: int New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
LayoutSaveSettings(toggleValue)
Parameters: toggleValue (int) – the new toggle value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)