WedmCutParameters Class

class NXOpen.CAM.WedmCutParameters

Bases: NXOpen.CAM.CutParameters

Represents a NXOpen.CAM.WedmCutParameters

New in version NX7.5.0.

Properties

Property Description
CheckIpwCollisions Returns or sets the value to Check for Ipw Collsions
CheckSafeClearance Returns the Check Safe Clearance
CutDirection Returns or sets the Cut Direction
HolderClearance Returns the Holder Clearance
Intol Returns or sets the intol value
IpwType Returns or sets the IPW type
LowerGuideOffset Returns the lower guide offset
LowerPlaneBuilder Returns the lower_plane builder
NeckClearance Returns the Neck Clearance
Outtol Returns or sets the outtol value
OverlapDistanceBuilder Returns the overlap_distance_builder
PartSafeClearance Returns the Part Safe Clearance
PartStock Returns the part stock
ShankClearance Returns the Shank Clearance
Tag Returns the Tag for this object.
Tolerances Returns the Tolerances builder
UpperGuideOffset Returns the upper guide offset
UpperPlaneBuilder Returns the upper_plane builder
UseToolHolder Returns or sets the use tool holder
WedmStepoverBuilder Returns the WedmStepover builder
WireDiameterBuilder Returns the wire_diameter builder
WirePosition Returns or sets the wire position

Methods

Enumerations

WedmCutParametersCutDirectionTypes Enumeration the types available for wedm cut direction
WedmCutParametersWirePositionTypes Enumeration the types available for wire position

Property Detail

CutDirection

WedmCutParameters.CutDirection

Returns or sets the Cut Direction

-------------------------------------

Getter Method

Signature CutDirection()

Returns:the Cut Direction
Return type:NXOpen.CAM.WedmCutParametersCutDirectionTypes

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

-------------------------------------

Setter Method

Signature CutDirection(cutDirection)

Parameters:cutDirection (NXOpen.CAM.WedmCutParametersCutDirectionTypes) – the Cut Direction

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

Intol

WedmCutParameters.Intol

Returns or sets the intol value

-------------------------------------

Getter Method

Signature Intol()

Returns:the intol value
Return type:float

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

-------------------------------------

Setter Method

Signature Intol(intol)

Parameters:intol (float) – the intol value

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

LowerGuideOffset

WedmCutParameters.LowerGuideOffset

Returns the lower guide offset

-------------------------------------

Getter Method

Signature LowerGuideOffset()

Returns:the lower guide offset
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

LowerPlaneBuilder

WedmCutParameters.LowerPlaneBuilder

Returns the lower_plane builder

-------------------------------------

Getter Method

Signature LowerPlaneBuilder()

Returns:the lower_plane Builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

Outtol

WedmCutParameters.Outtol

Returns or sets the outtol value

-------------------------------------

Getter Method

Signature Outtol()

Returns:the outol value
Return type:float

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

-------------------------------------

Setter Method

Signature Outtol(outtol)

Parameters:outtol (float) – the outol value

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

OverlapDistanceBuilder

WedmCutParameters.OverlapDistanceBuilder

Returns the overlap_distance_builder

-------------------------------------

Getter Method

Signature OverlapDistanceBuilder()

Returns:the overlap_distance_builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

UpperGuideOffset

WedmCutParameters.UpperGuideOffset

Returns the upper guide offset

-------------------------------------

Getter Method

Signature UpperGuideOffset()

Returns:the upper guide offset
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

UpperPlaneBuilder

WedmCutParameters.UpperPlaneBuilder

Returns the upper_plane builder

-------------------------------------

Getter Method

Signature UpperPlaneBuilder()

Returns:the upper_plane Builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

WedmStepoverBuilder

WedmCutParameters.WedmStepoverBuilder

Returns the WedmStepover builder

-------------------------------------

Getter Method

Signature WedmStepoverBuilder()

Returns:the Stepover Builder
Return type:NXOpen.CAM.StepoverBuilder

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

WireDiameterBuilder

WedmCutParameters.WireDiameterBuilder

Returns the wire_diameter builder

-------------------------------------

Getter Method

Signature WireDiameterBuilder()

Returns:the wire_diameter Builder
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

WirePosition

WedmCutParameters.WirePosition

Returns or sets the wire position

-------------------------------------

Getter Method

Signature WirePosition()

Returns:the wire position
Return type:NXOpen.CAM.WedmCutParametersWirePositionTypes

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

-------------------------------------

Setter Method

Signature WirePosition(wirePosition)

Parameters:wirePosition (NXOpen.CAM.WedmCutParametersWirePositionTypes) – the wire position

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)