WedmCutParametersCutDirectionTypes Enumeration

NXOpen.CAM.WedmCutParameters.CutDirectionTypes is an alias for NXOpen.CAM.WedmCutParametersCutDirectionTypes

class NXOpen.CAM.WedmCutParametersCutDirectionTypes

Bases: object

the types available for wedm cut direction

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Alternate
alternating cut direction
Clockwise
clockwise cut direction
CounterClockwise
counter clockwise cut direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.