NXOpen.CAE.ModelCheck.AlignShellElementNormalBuilder |
Represents a NXOpen.CAE.ModelCheck.AlignShellElementNormalBuilder builder used to align the normals of connected shell elements with a seed shell element. |
NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder |
Represents a NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder to check for duplicate elements within the candidate elements. |
NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder |
Represents a NXOpen.CAE.ModelCheck.DuplicateNodesCheckBuilder to check for duplicate nodes within the candidate nodes. |
NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilder |
Represents a NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilder which can be used to detect free element edges or non-manifold edges. |
NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilder |
Represents a NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilder used to check the material orientation for shell and solid elements. |
NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder |
Represents a NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder to perform quality checking on the candidate elements. |
NXOpen.CAE.ModelCheck.ElementQualityCheckResults |
Represents the element quality checking result of NXOpen.CAE.ModelCheck.ElementQualityCheckBuilder |
NXOpen.CAE.ModelCheck.ElementQualitySetting |
Represents element quality check settings of a specified solver language. |
NXOpen.CAE.ModelCheck.ElementQualitySettingCollection |
Represents a collection of NXOpen.CAE.ModelCheck.ElementQualitySetting in a cae part. |
NXOpen.CAE.ModelCheck.ElementSpecificTestValue |
Represents the quality setting for a specfied element reference |
NXOpen.CAE.ModelCheck.ElementTestResult |
Represents quality checking result for an element. |
NXOpen.CAE.ModelCheck.FaceClearanceCheckBuilder |
Represents a NXOpen.CAE.ModelCheck.FaceClearanceCheckBuilder to perform polygon face interference or clearance check. |
NXOpen.CAE.ModelCheck.ITestValue |
Represents the quality check criteria value settings |
NXOpen.CAE.ModelCheck.ModelSetupCheckBuilder |
Represents a NXOpen.CAE.ModelCheck.ModelSetupCheckBuilder which can be used to check if the active NXOpen.CAE.SimSolution contains all the necessary items for the analysis, including elements, loads, constraints and materials. |
NXOpen.CAE.ModelCheck.QualityTestValue |
Represents quality test settings of a specified test type |
NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder |
Represents a NXOpen.CAE.ModelCheck.ReverseShellElementNormalBuilder used to reverse normals for specified shell elements. |
NXOpen.CAE.ModelCheck.TestResult |
Represents quality checking result of a quality test |
NXOpen.CAE.ModelCheck.TestValueTypes |
Represents the quality check criteria value settings |