ElementTestResult Class¶
-
class
NXOpen.CAE.ModelCheck.
ElementTestResult
¶ Bases:
NXOpen.TransientObject
Represents quality checking result for an element.
To obtain an instance of this class use CAE.ModelCheck.ElementQualityCheckResults.GetElementTestResults
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
OverallResult | Returns the overrall result of this element. |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetTestResults | Returns the quality test results of this element @return |
Property Detail¶
OverallResult¶
-
ElementTestResult.
OverallResult
¶ Returns the overrall result of this element.
-------------------------------------
Getter Method
Signature
OverallResult()
Returns: Return type: NXOpen.CAE.ModelCheck.TestValueTypesResult
New in version NX8.5.0.
License requirements: None.
Method Detail¶
Dispose¶
-
ElementTestResult.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.5.0.
License requirements: None.
GetTestResults¶
-
ElementTestResult.
GetTestResults
¶ Returns the quality test results of this element
Signature
GetTestResults()
Returns: Return type: list of NXOpen.CAE.ModelCheck.TestResult
New in version NX8.5.0.
License requirements: None.