TestValueTypesResult Enumeration¶
NXOpen.CAE.ModelCheck.TestValueTypes.Result is an alias for NXOpen.CAE.ModelCheck.TestValueTypesResult
-
class
NXOpen.CAE.ModelCheck.
TestValueTypesResult
¶ Bases:
object
the checking result
Enum Members
Enum Member Enum Member Description Passed indicates the test value does not violate the criteria valuesFailed indicates the test value violates the error criteria valueException indicates there is an exception thrown during the checkingNotApply indicates the test is not available or not done for an elementWarned indicates the test value violates the warning criteria value-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-