TestValueTypesTestType Enumeration¶
NXOpen.CAE.ModelCheck.TestValueTypes.TestType is an alias for NXOpen.CAE.ModelCheck.TestValueTypesTestType
-
class
NXOpen.CAE.ModelCheck.
TestValueTypesTestType
¶ Bases:
object
the test types
Enum Members
check consistent Y. When elements are modeled in XY plane, check consistent Z.”
“AxisymmetricX”, ” When elements are modeled in XZ plane,check X >= 0.0. When elements are modeled in XY plane, check Y >= 0.0.”
“AspectRatio”, ” - ” “SkewAngle”, ” - ” “InteriorAngleMinimum”, ” - ” “InteriorAngleMaximum”, ” - ” “Taper”, ” - ” “WarpFactor”, ” - ” “FaceWarpCoefficient”, ” - ” “EdgePointLengthRatio”, ” - ” “EdgePointIncludedAngle”, ” - ” “LengthRatioOffset”, ” - ” “ParallelDeviation”, ” - ” “ShapeFactor”, ” - ” “Twist”, ” - ” “LengthMinimum”, ” - ” “LengthMaximum”, ” - ” “TetCollapse”, ” - ” “WarpageAngle”, ” - ” “CohesiveElement”, ” - “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-