DuplicateElementsCheckBuilderDeletePreference Enumeration¶
NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.DeletePreference is an alias for NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilderDeletePreference
-
class
NXOpen.CAE.ModelCheck.
DuplicateElementsCheckBuilderDeletePreference
¶ Bases:
object
Represents the duplicate elements deleting preference
Enum Members
NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.PreferenceElements`
“- “RemoveSelected”, ” Delete the elements specified in the element list
NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.PreferenceElements`
“-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.