TestValueTypesElementReference_Struct Struct¶
NXOpen.CAE.ModelCheck.TestValueTypes.ElementReference is an alias for NXOpen.CAE.ModelCheck.TestValueTypesElementReference_Struct
-
class
NXOpen.CAE.ModelCheck.
TestValueTypesElementReference_Struct
¶ Bases:
object
represents an element reference definition associated with this test
Fields¶
Field | Description |
---|---|
ElementTypeName | the element type name, which is defined in solver specific item |
ElementPropertyName | a specified integer element property name |
ElementPropertyValue | the control value of integer element property, only valid when property name is not NULL |
ElementTypeName¶
-
TestValueTypesElementReference_Struct.
ElementTypeName
¶ the element type name, which is defined in solver specific item
-------------------------------------
Getter Method Signature
ElementTypeName()
Returns: Return type: str -------------------------------------
Setter Method
Signature
ElementTypeName(value)
Parameters: value (str) –
ElementPropertyName¶
-
TestValueTypesElementReference_Struct.
ElementPropertyName
¶ a specified integer element property name
-------------------------------------
Getter Method Signature
ElementPropertyName()
Returns: Return type: str -------------------------------------
Setter Method
Signature
ElementPropertyName(value)
Parameters: value (str) –
ElementPropertyValue¶
-
TestValueTypesElementReference_Struct.
ElementPropertyValue
¶ the control value of integer element property, only valid when property name is not NULL
-------------------------------------
Getter Method Signature
ElementPropertyValue()
Returns: Return type: int -------------------------------------
Setter Method
Signature
ElementPropertyValue(value)
Parameters: value (int) –