ElementQualitySetting Class¶
-
class
NXOpen.CAE.ModelCheck.
ElementQualitySetting
¶ Bases:
NXOpen.TaggedObject
Represents element quality check settings of a specified solver language. Each solve language has a
NXOpen.CAE.ModelCheck.ElementQualitySetting
.To get a quality check criteria value of a specfied quality test for one element, you can call
NXOpen.CAE.ModelCheck.ElementQualitySetting.LocateTestDescriptorName
to get the test criteria value name, then callNXOpen.CAE.ModelCheck.ElementQualitySetting.GetQualityValue
to get the criteria value object.Not to support KF
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
LimitValueOption | Returns or sets the limit value option |
Tag | Returns the Tag for this object. |
TestValueCount | Returns the count of NXOpen.CAE.ModelCheck.QualityTestValue in the setting |
UseElementSpecificValue | Returns or sets an option indicating whether to use element specific quality value for testing |
Methods¶
Method | Description |
---|---|
GetQualityValue | Returns the test quality value with the specified descriptor name @return |
GetTestValueByIndex | Returns the NXOpen.CAE.ModelCheck.QualityTestValue at the specified index in the setting @return |
GetTestValueByType | Returns the NXOpen.CAE.ModelCheck.QualityTestValue of a specified NXOpen.CAE.ModelCheck.TestValueTypesTestType @return |
LocateTestDescriptorName | Returns the name of a quality test value, which is associated with an element for a specified test type @return |
ResetToCustomerDefault | Reset the quality check setting as customer default |
Enumerations¶
ElementQualitySettingLimitValue Enumeration | indicates how criteria value is defined |
Property Detail¶
LimitValueOption¶
-
ElementQualitySetting.
LimitValueOption
¶ Returns or sets the limit value option
-------------------------------------
Getter Method
Signature
LimitValueOption()
Returns: Return type: NXOpen.CAE.ModelCheck.ElementQualitySettingLimitValue
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitValueOption(limitValueOption)
Parameters: limitValueOption ( NXOpen.CAE.ModelCheck.ElementQualitySettingLimitValue
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
TestValueCount¶
-
ElementQualitySetting.
TestValueCount
¶ Returns the count of
NXOpen.CAE.ModelCheck.QualityTestValue
in the setting-------------------------------------
Getter Method
Signature
TestValueCount()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
UseElementSpecificValue¶
-
ElementQualitySetting.
UseElementSpecificValue
¶ Returns or sets an option indicating whether to use element specific quality value for testing
-------------------------------------
Getter Method
Signature
UseElementSpecificValue()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseElementSpecificValue(useElementSpecificValue)
Parameters: useElementSpecificValue (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
GetQualityValue¶
-
ElementQualitySetting.
GetQualityValue
¶ Returns the test quality value with the specified descriptor name
Signature
GetQualityValue(descriptorName)
Parameters: descriptorName (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: NXOpen.CAE.ModelCheck.ITestValue
New in version NX8.5.0.
License requirements: None.
GetTestValueByIndex¶
-
ElementQualitySetting.
GetTestValueByIndex
¶ Returns the
NXOpen.CAE.ModelCheck.QualityTestValue
at the specified index in the settingSignature
GetTestValueByIndex(index)
Parameters: index (int) – Returns: Return type: NXOpen.CAE.ModelCheck.QualityTestValue
New in version NX8.5.0.
License requirements: None.
GetTestValueByType¶
-
ElementQualitySetting.
GetTestValueByType
¶ Returns the
NXOpen.CAE.ModelCheck.QualityTestValue
of a specifiedNXOpen.CAE.ModelCheck.TestValueTypesTestType
Signature
GetTestValueByType(testType)
Parameters: testType ( NXOpen.CAE.ModelCheck.TestValueTypesTestType
) –Returns: Return type: NXOpen.CAE.ModelCheck.QualityTestValue
New in version NX8.5.0.
License requirements: None.
LocateTestDescriptorName¶
-
ElementQualitySetting.
LocateTestDescriptorName
¶ Returns the name of a quality test value, which is associated with an element for a specified test type
Signature
LocateTestDescriptorName(element, testType, useElemSpecific)
Parameters: - element (
NXOpen.CAE.FEElement
) – - testType (
NXOpen.CAE.ModelCheck.TestValueTypesTestType
) – - useElemSpecific (bool) –
Returns: Return type: str
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- element (