Solid Edge FrameworkSupport Type Library
Dimension Object Members
Overview 
Public Methods
Public Method AddProjectionLineBreaks
Public Method BreakAlignmentSetBreaks the alignment set and allows the dimensions to move independently.
Public Method BringForwardChanges the display order of the referenced object by moving it in front of the first object that obscures it.
Public Method BringToFrontChanges the display order of the referenced object by moving it in front of all other overlapping objects.
Public Method ClearProjectionLineBreaksThis method clears the list of breaking dimensions.
Public Method CopyPlaces a copy of the referenced object on the clipboard.
Public Method CutMoves the referenced object.
Public Method DeleteDeletes the referenced object.
Public Method GetCommentReturns the variable table comment.
Public Method GetDiscreteValuesReturns discrete values and number of discrete values of the referenced dimension object.
Public Method GetDisplayDataThis method returns available display data for the referenced Dimension object.
Public Method GetJogPoint1DistanceReturns the JogPoint1 distance for the jogged line in a Dimension.
Public Method GetJogPoint2Returns the JogPoint2 distance for the jogged line in a Dimension.
Public Method GetJogPoint3DistanceSets the JogPoint3 distance for the jogged line in a Dimension.
Public Method GetKeyPointReturns information about a specified key point.
Public Method GetMultipleJogPointsSets and returns number and offsets of jog points of the referenced dimension object.
Public Method GetRelatedReturns the related object at the specified index.
Public Method GetRelatedCountReturns the number of objects to which the referenced Dimension is related.
Public Method GetTextOffsetsReturns the offsets for the dimension text of the referenced Dimension object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReattachToDrawingViewReattaches the referenced dimension to a specified drawing view and returns the status after reattach.
Public Method RemoveFromAlignmentSetRemoves the dimension from alignment set
Public Method SelectSelects the referenced object in the active window.
Public Method SendBackwardChanges the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Public Method SendToBackChanges the display order of visible objects by moving the referenced object behind all overlapping objects.
Public Method SetCommentSets the variable table comment.
Public Method SetDiscreteValuesSets discrete values to the referenced dimension object.
Public Method SetJogPoint1DistanceSets the JogPoint1 distance for the jogged line in a Dimension.
Public Method SetJogPoint2Sets the JogPoint2 distance for the jogged line in a Dimension.
Public Method SetJogPoint3DistanceSets the JogPoint3 distance for the jogged line in a Dimension.
Public Method SetKeyPointSets the position for a specified key point.
Public Method SetMultipleJogPointsSets and returns number and offsets of jog points of the referenced dimension object.
Public Method SetPMIEditDirectionSet the edit direction of the PMI dimension. The input constant determines which direction to move on edit value.
Public Method SetTextOffsetsSets the offsets for the dimension text of the referenced Dimension object.
Public Method UpdateStatusUpdates the reference dimension object and returns its status after update.
Public Properties
Public Property AbsoluteTrackDistance
Public Property AngleClockwiseReturns True if the referenced Dimension object measures the angle clockwise.
Public Property AngleComplimentSpecifies whether or not the referenced dimension measures the compliment value.
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property AxisSets and returns the object used as the axis for the referenced object. It must be a line.
Public Property BreakDistanceSets and returns the break distance for the referenced Dimension object.
Public Property BreakPositionSets and returns the break position for the referenced Dimension object.
Public Property ChamferDimensionModeReturns the mode of chamfer dimension (along axis, callout perpendicular, or callout parallel).
Public Property ConstraintSets and returns the Constraint property for the referenced dimension object.
Public Property DimensionTypeSets and returns the type of dimension for the referenced object.
Public Property DisplayHalfSets and returns the Display Half flag for symmetrical and radial diameter dimensions.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property DisplayTypeSets and returns the display type for the referenced object.
Public Property DocumentReturns the document to which the referenced object belongs.
Public Property Expose
Public Property ExposeNameThis read-write String property sets and returns the name of the referenced object when the object is exposed as a custom property.
Public Property FormulaSets and returns the formula of the referenced Variable object.
Public Property GroupMemberTypeReturns the type of group(Stack, Chain, Coordinate or Not a Group) to which referenced dimension object belongs.
Public Property HidePMIShow or Hide the referenced PMI Dimension object.
Public Property HoleClassStringHole Class String. This string must match a class in the standards table, e.g. H7.
Public Property IndexReturns the numeric index for the active object.
Public Property InhibitZeroToleranceDisplayInhibit display of zero tolerance value
Public Property InspectionDetermines whether or not an inspection bubble is applied to the referenced Dimension object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property JoggedSpecifies whether or not the referenced Dimension object is jogged.
Public Property KeyReturns a key (a string) to find the object relative to its owning parents.
Public Property KeyPointCountReturns the number of keypoints/handles that are supported by the referenced object.
Public Property LayerSets and returns the named layer on which the referenced object resides.
Public Property LeaderSpecifies whether or not the referenced object has a leader line.
Public Property LeaderDistanceSets and returns the leader distance of the referenced Dimension object.
Public Property MeasureLineDirectionDetermines the direction of measurement for coordinate dimensions.
Public Property MeasurementAxisDirectionSpecifies the direction in which the linear distance is measured for the referenced Dimension object.
Public Property MeasurementAxisExSets and returns the axis mode of a Dimension.
Public Property NameReturns the name of the referenced object.
Public Property OffsetLeaderSpecifies whether or not the referenced Dimension object has the offset leader line.
Public Property OriginLineDirectionSpecifies the orientation of the origin line for coordinate dimensions.
Public Property OverrideChamferAngleStringReturns the chamfer dimension angle override string.
Public Property OverrideStringSets and returns the override value set on the referenced Dimension object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PMIPlane
Public Property PMITrackDistance
Public Property PrefixDisplayedTextReturns the evaluated Prefix text.
Public Property PrefixInsideSpecifies whether or not prefix text for the referenced Dimension object is placed inside the associated basic dimension or inspection box.
Public Property PrefixStringSets and returns the prefix string to be displayed along with the dimension text.
Public Property PrimaryLowerToleranceSets and returns the text for the primary lower tolerance value.
Public Property PrimaryToleranceSymbolSets and returns the text for the primary tolerance symbol of the referenced Dimension object.
Public Property PrimaryUpperToleranceSets and returns the text for the primary upper tolerance value.
Public Property ProjectionArcSets and returns the projection arc for the referenced Dimension object.
Public Property ProjectionLineAngle1They return double values that represent the angle between the projection line and the x-axis of the sheet.
Public Property ProjectionLineAngle2They return double values that represent the angle between the projection line and the x-axis of the sheet.
Public Property ProjectionLineDirectionSpecifies the projection line direction.
Public Property RadialExtensionDistanceSets and returns the extension distance of radial and half displayed diameter dimensions. Negative is away from the terminator.
Public Property SecondaryLowerToleranceSets and returns the text for the secondary lower tolerance value.
Public Property SecondaryUpperToleranceSets and returns the text for the secondary upper tolerance value.
Public Property SecondValueReturns the chamfer dimension angle.
Public Property ShaftClassStringShaft Class String. This string must match a class in the standards table, e.g. h7.
Public Property StatusOfDimensionReturns the status(Detached, Error, Driving, Driven) of the referenced dimension object.
Public Property StyleSets and returns the active style on dimension
Public Property Subfix2DisplayedTextReturns the evaluated Subfix2 text.
Public Property SubfixAlignment
Public Property SubfixDisplayedTextReturns the evaluated Subfix text.
Public Property SubfixStringSets and returns the subfix text to be displayed along with the dimension text.
Public Property SubfixString2Sets and returns the subfix2 text to be displayed along with the dimension text.
Public Property SuffixDisplayedTextReturns the evaluated Suffix text.
Public Property SuffixStringSets and returns the suffix string to be displayed along with the dimension text.
Public Property SuperfixDisplayedTextReturns the evaluated Superfix text.
Public Property SuperfixStringSets and returns the superfix text to be displayed along with the dimension text.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TerminatorPositionDetermines the position (inside or outside of the projection lines) of the terminator for the referenced Dimension object.
Public Property TextScaleSets and returns the text scale of the object.
Public Property TrackAngleSets and returns the angle between the referenced Dimension object and the object it measures.
Public Property TrackDistanceSets and returns the track distance of the referenced Dimension object.
Public Property True3DSketchDimensionSets and returns the True3DSketchDimension property for the referenced dimension object.
Public Property TypeSpecifies the type of the object being referenced.
Public Property UseStandardLimitAndFitToleranceExtract tolerances from standards tables when TRUE. Use user-defined tolerances when FALSE. When TRUE, use appropriate DisplayType and use HoleClass and/or ShaftClass properties.
Public Property ValueSets or returns the value of the referenced Dimension object.
Public Property VariableTableNameReturns the name used in the variable table.
Public Property ZOrderSpecifies the front-to-back order in which an object is displayed relative to other objects.
See Also

Dimension Object