Solid Edge FrameworkSupport Type Library
OverrideChamferAngleString Property
Description
Returns the chamfer dimension angle override string.
Property type
Read-write property
Syntax
Visual Basic
Public Property OverrideChamferAngleString As String
Remarks
When the override string is set, the chamfer dimension displays this text string instead of the computed dimension value.
See Also

Dimension Object  | Dimension Members