Solid Edge FrameworkSupport Type Library
SendBackward Method
Description
Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display but when you do not want to send the object all the way to the back of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objArc As SolidEdgeFrameworkSupport.Arc2d
    Dim objDimension1 As SolidEdgeFrameworkSupport.Dimension
    Dim objDimension2 As SolidEdgeFrameworkSupport.Dimension
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create an arc2d
    Set objArc = objSheet.Arcs2d.AddByCenterStartEnd(xCenter:=0.2, _
                                                     yCenter:=0.2, xStart:=0.1, yStart:=0.1, xEnd:=0.3, yEnd:=0.3)
    'create 2 dimensions
    Set objDimension1 = objSheet.Dimensions.AddLength(Object:=objArc)
    Set objDimension2 = objSheet.Dimensions.AddAngle(Object:=objArc)
    'Send the second dimension backward
    objDimension2.SendBackward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDimension1 = Nothing
    Set objDimension2 = Nothing
    Set objArc = Nothing
End Sub
See Also

Dimension Object  | Dimension Members