Solid Edge FrameworkSupport Type Library
GetComment Method
Description
Returns the variable table comment.
Syntax
Visual Basic
Public Function GetComment() As String
Example
Imports System.Runtime.InteropServices
Public Class Form1
    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApp As SolidEdgeFramework.Application = Nothing
        Dim objDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objSheets As SolidEdgeDraft.Sheets = Nothing
        Dim objDimensions As SolidEdgeFrameworkSupport.Dimensions = Nothing
        Dim objHzDim As SolidEdgeFrameworkSupport.Dimension = Nothing
        Dim objLines As SolidEdgeFrameworkSupport.Lines2d = Nothing
        Dim objHzLine As SolidEdgeFrameworkSupport.Line2d = Nothing
        Dim strComment As String
        Try
            ' Create/get the application with specific settings
            objApp = Marshal.GetActiveObject("SolidEdge.Application")

            If objApp Is Nothing Then
                objApp = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
                objApp.Visible = True
            End If

            objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
            'Get the sheets collection
            objSheets = objDoc.Sheets

            'Get the active sheet
            objSheet = objDoc.ActiveSheet

            'Get the lines collection and dimensions collection.
            objLines = objSheet.Lines2d
            objDimensions = objSheet.Dimensions

            'Add a horizontal line and a vertical line
            objHzLine = objLines.AddBy2Points(x1:=0.2, y1:=0.2, x2:=0.3, y2:=0.2)

            'Add dimensions to the lines that are created above.
            objHzDim = objDimensions.AddLength(Object:=objHzLine)

            'set the Comment
            objHzDim.SetComment("LineLength")

            'get the comment
            strComment = objHzDim.GetComment

        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try


    End Sub
End Class
See Also

Dimension Object  | Dimension Members