Solid Edge FrameworkSupport Type Library
LeaderDistance Property
Description
Sets and returns the leader distance of the referenced Dimension object.
Property type
Read-write property
Syntax
Visual Basic
Public Property LeaderDistance As Double
Remarks
The leader distance defines the leader point at the text position. The leader line is valid only when the break is positioned to left or right of the Dimension object.
See Also

Dimension Object  | Dimension Members