Solid Edge FrameworkSupport Type Library
TrackAngle Property
Description
Sets and returns the angle between the referenced Dimension object and the object it measures.
Property type
Read-write property
Syntax
Visual Basic
Public Property TrackAngle As Double
Remarks
The track angle defines the angle between the circular diameter dimension line and the x-axis. The value returned is in radians. For dimension types other than circular diameter, -99 is returned.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCircle As SolidEdgeFrameworkSupport.Circle2d
    Dim objDim As SolidEdgeFrameworkSupport.Dimension
    Dim dblTraAng As Double
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a line
    Set objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.3, y:=0.3, Radius:=0.1)
    'create a dimension object
    Set objDim = objSheet.Dimensions.AddCircularDiameter(Object:=objCircle)
    'get TrackAngle
    dblTraAng = objDim.TrackAngle
    'set TrackAngle
    objDim.TrackAngle = 0.3
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCircle = Nothing
    Set objDim = Nothing
End Sub
See Also

Dimension Object  | Dimension Members