InspectionMethodBuilder Class¶
-
class
NXOpen.CAM.
InspectionMethodBuilder
¶ Bases:
NXOpen.CAM.MethodBuilder
Represents the builder for a CMM Inspection method.
To create a new instance of this class, use
NXOpen.CAM.InspectionGroupCollection.CreateInspectionMethodBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AdvanceAngle | Returns or sets the advance angle (degrees) |
AngleMode | Returns or sets the polar angle mode |
AngularPointCount | Returns or sets the number of points in angular direction |
ApproachDistance | Returns or sets the approach distance |
AxisExtrapolationMode | Returns or sets the analysis axis extrapolation mode |
CircularScan | Returns or sets a flag to indicate if scan arc is allowed |
ColorApproach | Returns or sets the color used for displaying approach elements |
ColorEntryExit | Returns or sets the color used for displaying entry and exit elements |
ColorLine | Returns or sets the color used for displaying path lines |
ColorMeasurePoint | Returns or sets the color used for displaying measured points |
ColorRetract | Returns or sets the color used for displaying retract elements |
ColorTransition | Returns or sets the color used for displaying transition elements |
CurvatureFactor | Returns or sets the curvature increase factor |
CurveScan | Returns or sets a flag to indicate if scan curve is allowed |
CutParameters | Returns the cut parameter object |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
CylinderCircleFitMode | Returns or sets the analysis cylinder/circle fitting mode |
DatumPlaneFittingMode | Returns or sets the analysis datum plane fitting mode |
DefaultOperationType | Returns or sets the default inspection operation type |
DepthDistance | Returns or sets the depth distance |
Description | Returns or sets the description |
EndDistance | Returns or sets the end point offset distance along the scan |
EndPercentage | Returns or sets the end Percentage along the scan |
EndUdeSet | Returns the end ude set |
EntryAvoidance | Returns or sets a flag to indicate if collision avoidance is required at entry |
EntryExitDistance | Returns or sets the distance from the entry or exit point to safe plane |
EntryPoint | Returns or sets a flag to indicate if an entry point is required |
EntryTransition | Returns or sets the type of entry transition |
ExitAvoidance | Returns or sets a flag to indicate if collision avoidance is required at exit |
ExitPoint | Returns or sets a flag to indicate if an exit point is required |
ExitTransition | Returns or sets the type of exit transition |
FeatureOffsetDistance | Returns or sets the offset feature distance |
InspectionMode | Returns or sets the default inspection mode |
LimitsOfSizeMode | Returns or sets the analysis limits of size fitting mode |
LineScan | Returns or sets a flag to indicate if scan line is allowed |
ManualPoint | Returns or sets a flag to indicate if manual point creation is allowed |
MaxSpacing | Returns or sets the maximum spacing between scan points |
MaximumRadius | Returns or sets the maximum radius |
MaximumRadiusMode | Returns or sets the maximum radius mode |
MethodType | Returns or sets the method feature type |
MinSpacing | Returns or sets the minimum spacing between scan points |
MinimumRadius | Returns or sets the minimum radius |
MinimumRadiusMode | Returns or sets the minimum radius mode |
NbScanPoints | Returns or sets the minimum number of scan points |
OffsetDistance | Returns or sets the offset distance |
OffsetEndAngle | Returns or sets the offset from end angle |
OffsetMaximumRadius | Returns or sets the offset from maximum radius |
OffsetMinimumRadius | Returns or sets the offset from minimum radius |
OffsetStartAngle | Returns or sets the offset from start angle |
OptimizationMethod | Returns or sets the optim method |
PaintDisplay | Returns the sub builder for paint display |
PathDisplay | Returns the sub builder for path display |
PathDisplayColors | Returns the sub builder for path display colors |
Pitch | Returns or sets the pitch of the Scan Helix |
PointCount | Returns or sets the number of path points |
PointHelix | Returns or sets a flag to indicate if point helix is allowed |
PointSequenceDirection | Returns or sets the point sequence start direction |
PointSequenceMode | Returns or sets the point sequence mode |
PointSequenceStart | Returns or sets the point sequence start location |
PolarGrid | Returns or sets a flag to indicate if circular point grid is allowed |
PolarPointSequence | Returns or sets the polar point sequence mode |
PolarSequenceDirection | Returns or sets the polar sequence direction |
PolarSequenceStart | Returns or sets the polar sequence start location |
ProbeTipType | Returns or sets the preferred probe tip type |
ProfileDispositionMode | Returns or sets the analysis profile disposition fitting mode |
RadialPointCount | Returns or sets the number of points in radial direction |
ReferenceFeatureMode | Returns or sets the relative measurement mode |
ReferenceFeatureOffsetDistance | Returns or sets the offset distance for relative measurement |
ReferenceFeaturePointCount | Returns or sets the number of points for relative measurement |
ReferenceFeatureZoneRadius | Returns or sets the zone radius for relative measurement |
RetractDistance | Returns or sets the retract distance |
Revolutions | Returns or sets the revolutions of the Scan Helix |
ScanCurveMode | Returns or sets the scan curve mode |
ScanForce | Returns or sets the scan force |
ScanModeType | Returns or sets the 3,5 axis scan mode type |
ScanSpeed | Returns or sets the scan speed |
SensorStrategy | Returns or sets the sensor selection strategy |
SilhouDisplay | Returns the sub builder for silhou display |
Speed | Returns or sets the default animation speed setting |
StartDistance | Returns or sets the start point offset distance along the scan |
StartEndMode | Returns or sets the scan start end mode |
StartPercentage | Returns or sets the start percentage along the scan |
StartUdeSet | Returns the start ude set |
StepSize | Returns or sets the scan step size |
StopRadius | Returns or sets the scan stop radius |
SurfaceProfileMode | Returns or sets the analysis surface profile fitting mode |
Sweep | Returns or sets the sweep of the Scan Helix |
Tag | Returns the Tag for this object. |
TiltAngle | Returns or sets the tilt angle (degrees) |
ToolDisplay | Returns the sub builder for tool display |
TurnDirection | Returns or sets the turn direction type of the Scan Helix |
TurnType | Returns or sets the turn type of the Scan Helix |
UCount | Returns or sets the number of points in U direction |
UEnd | Returns or sets the U end parameter |
UEndDeg | Returns or sets the U end degrees |
UEndDist | Returns or sets the U end distance |
UEndMode | Returns or sets the end U mode |
UEndSweep | Returns or sets the U sweep degrees |
UStart | Returns or sets the U start parameter |
UStartDeg | Returns or sets the U start degrees |
UStartDist | Returns or sets the U start distance |
UStartMode | Returns or sets the start U mode |
UStartSweep | Returns or sets the U start sweep degrees |
UVGrid | Returns or sets a flag to indicate if rectangular UV grid is allowed |
VCount | Returns or sets the number of points in V direction |
VEnd | Returns or sets the V end parameter |
VEndDeg | Returns or sets the V end degrees |
VEndDist | Returns or sets the V end distance |
VEndMode | Returns or sets the end V mode |
VEndSweep | Returns or sets the V sweep degrees |
VStart | Returns or sets the V start parameter |
VStartDeg | Returns or sets the V start degrees |
VStartDist | Returns or sets the V start distance |
VStartMode | Returns or sets the start V mode |
VStartSweep | Returns or sets the V start sweep degrees |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetCutMethod | Get cut method |
GetObject | Returns the object currently being edited by this builder. |
SetCutMethod | Set cut method |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AdvanceAngle¶
-
InspectionMethodBuilder.
AdvanceAngle
¶ Returns or sets the advance angle (degrees)
-------------------------------------
Getter Method
Signature
AdvanceAngle
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdvanceAngle
Parameters: angle (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AngleMode¶
-
InspectionMethodBuilder.
AngleMode
¶ Returns or sets the polar angle mode
-------------------------------------
Getter Method
Signature
AngleMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPolarAngleModeTypes
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderPolarAngleModeTypes
) –New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AngularPointCount¶
-
InspectionMethodBuilder.
AngularPointCount
¶ Returns or sets the number of points in angular direction
-------------------------------------
Getter Method
Signature
AngularPointCount
Returns: Return type: int New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularPointCount
Parameters: ptCount (int) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ApproachDistance¶
-
InspectionMethodBuilder.
ApproachDistance
¶ Returns or sets the approach distance
-------------------------------------
Getter Method
Signature
ApproachDistance
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApproachDistance
Parameters: distance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AxisExtrapolationMode¶
-
InspectionMethodBuilder.
AxisExtrapolationMode
¶ Returns or sets the analysis axis extrapolation mode
-------------------------------------
Getter Method
Signature
AxisExtrapolationMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderAxisExtrapolationTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisExtrapolationMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderAxisExtrapolationTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CircularScan¶
-
InspectionMethodBuilder.
CircularScan
¶ Returns or sets a flag to indicate if scan arc is allowed
-------------------------------------
Getter Method
Signature
CircularScan
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircularScan
Parameters: circularScan (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorApproach¶
-
InspectionMethodBuilder.
ColorApproach
¶ Returns or sets the color used for displaying approach elements
-------------------------------------
Getter Method
Signature
ColorApproach
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorApproach
Parameters: colorApproach (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorEntryExit¶
-
InspectionMethodBuilder.
ColorEntryExit
¶ Returns or sets the color used for displaying entry and exit elements
-------------------------------------
Getter Method
Signature
ColorEntryExit
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorEntryExit
Parameters: colorEntryExit (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorLine¶
-
InspectionMethodBuilder.
ColorLine
¶ Returns or sets the color used for displaying path lines
-------------------------------------
Getter Method
Signature
ColorLine
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorLine
Parameters: colorLine (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorMeasurePoint¶
-
InspectionMethodBuilder.
ColorMeasurePoint
¶ Returns or sets the color used for displaying measured points
-------------------------------------
Getter Method
Signature
ColorMeasurePoint
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorMeasurePoint
Parameters: colorMeasurePoint (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorRetract¶
-
InspectionMethodBuilder.
ColorRetract
¶ Returns or sets the color used for displaying retract elements
-------------------------------------
Getter Method
Signature
ColorRetract
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorRetract
Parameters: colorRetract (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ColorTransition¶
-
InspectionMethodBuilder.
ColorTransition
¶ Returns or sets the color used for displaying transition elements
-------------------------------------
Getter Method
Signature
ColorTransition
Returns: Return type: Id New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorTransition
Parameters: colorTransition (Id) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CurvatureFactor¶
-
InspectionMethodBuilder.
CurvatureFactor
¶ Returns or sets the curvature increase factor
-------------------------------------
Getter Method
Signature
CurvatureFactor
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurvatureFactor
Parameters: curvatureFactor (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CurveScan¶
-
InspectionMethodBuilder.
CurveScan
¶ Returns or sets a flag to indicate if scan curve is allowed
-------------------------------------
Getter Method
Signature
CurveScan
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveScan
Parameters: curveScan (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CylinderCircleFitMode¶
-
InspectionMethodBuilder.
CylinderCircleFitMode
¶ Returns or sets the analysis cylinder/circle fitting mode
-------------------------------------
Getter Method
Signature
CylinderCircleFitMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderCylinderFittingTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CylinderCircleFitMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderCylinderFittingTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DatumPlaneFittingMode¶
-
InspectionMethodBuilder.
DatumPlaneFittingMode
¶ Returns or sets the analysis datum plane fitting mode
-------------------------------------
Getter Method
Signature
DatumPlaneFittingMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderDatumPlaneFittingTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumPlaneFittingMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderDatumPlaneFittingTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DefaultOperationType¶
-
InspectionMethodBuilder.
DefaultOperationType
¶ Returns or sets the default inspection operation type
-------------------------------------
Getter Method
Signature
DefaultOperationType
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderOperationTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultOperationType
Parameters: operationType ( NXOpen.CAM.InspectionMethodBuilderOperationTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthDistance¶
-
InspectionMethodBuilder.
DepthDistance
¶ Returns or sets the depth distance
-------------------------------------
Getter Method
Signature
DepthDistance
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthDistance
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndDistance¶
-
InspectionMethodBuilder.
EndDistance
¶ Returns or sets the end point offset distance along the scan
-------------------------------------
Getter Method
Signature
EndDistance
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndDistance
Parameters: endDistance (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndPercentage¶
-
InspectionMethodBuilder.
EndPercentage
¶ Returns or sets the end Percentage along the scan
-------------------------------------
Getter Method
Signature
EndPercentage
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPercentage
Parameters: endPercentage (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EntryAvoidance¶
-
InspectionMethodBuilder.
EntryAvoidance
¶ Returns or sets a flag to indicate if collision avoidance is required at entry
-------------------------------------
Getter Method
Signature
EntryAvoidance
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EntryAvoidance
Parameters: entryAvoidance (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EntryExitDistance¶
-
InspectionMethodBuilder.
EntryExitDistance
¶ Returns or sets the distance from the entry or exit point to safe plane
-------------------------------------
Getter Method
Signature
EntryExitDistance
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EntryExitDistance
Parameters: entryExitDistance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EntryPoint¶
-
InspectionMethodBuilder.
EntryPoint
¶ Returns or sets a flag to indicate if an entry point is required
-------------------------------------
Getter Method
Signature
EntryPoint
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EntryPoint
Parameters: entryPoint (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EntryTransition¶
-
InspectionMethodBuilder.
EntryTransition
¶ Returns or sets the type of entry transition
-------------------------------------
Getter Method
Signature
EntryTransition
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderTransitionTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EntryTransition
Parameters: entryTransition ( NXOpen.CAM.InspectionMethodBuilderTransitionTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExitAvoidance¶
-
InspectionMethodBuilder.
ExitAvoidance
¶ Returns or sets a flag to indicate if collision avoidance is required at exit
-------------------------------------
Getter Method
Signature
ExitAvoidance
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExitAvoidance
Parameters: exitAvoidance (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExitPoint¶
-
InspectionMethodBuilder.
ExitPoint
¶ Returns or sets a flag to indicate if an exit point is required
-------------------------------------
Getter Method
Signature
ExitPoint
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExitPoint
Parameters: exitPoint (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ExitTransition¶
-
InspectionMethodBuilder.
ExitTransition
¶ Returns or sets the type of exit transition
-------------------------------------
Getter Method
Signature
ExitTransition
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderTransitionTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExitTransition
Parameters: exitTransition ( NXOpen.CAM.InspectionMethodBuilderTransitionTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FeatureOffsetDistance¶
-
InspectionMethodBuilder.
FeatureOffsetDistance
¶ Returns or sets the offset feature distance
-------------------------------------
Getter Method
Signature
FeatureOffsetDistance
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureOffsetDistance
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
InspectionMode¶
-
InspectionMethodBuilder.
InspectionMode
¶ Returns or sets the default inspection mode
-------------------------------------
Getter Method
Signature
InspectionMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderInspectionModes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InspectionMode
Parameters: inspectionMode ( NXOpen.CAM.InspectionMethodBuilderInspectionModes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LimitsOfSizeMode¶
-
InspectionMethodBuilder.
LimitsOfSizeMode
¶ Returns or sets the analysis limits of size fitting mode
-------------------------------------
Getter Method
Signature
LimitsOfSizeMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderLimitsOfSizeTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitsOfSizeMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderLimitsOfSizeTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LineScan¶
-
InspectionMethodBuilder.
LineScan
¶ Returns or sets a flag to indicate if scan line is allowed
-------------------------------------
Getter Method
Signature
LineScan
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineScan
Parameters: lineScan (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ManualPoint¶
-
InspectionMethodBuilder.
ManualPoint
¶ Returns or sets a flag to indicate if manual point creation is allowed
-------------------------------------
Getter Method
Signature
ManualPoint
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ManualPoint
Parameters: manualPoint (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaxSpacing¶
-
InspectionMethodBuilder.
MaxSpacing
¶ Returns or sets the maximum spacing between scan points
-------------------------------------
Getter Method
Signature
MaxSpacing
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxSpacing
Parameters: maxSpacing (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaximumRadius¶
-
InspectionMethodBuilder.
MaximumRadius
¶ Returns or sets the maximum radius
-------------------------------------
Getter Method
Signature
MaximumRadius
Returns: Return type: float New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumRadius
Parameters: radius (float) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaximumRadiusMode¶
-
InspectionMethodBuilder.
MaximumRadiusMode
¶ Returns or sets the maximum radius mode
-------------------------------------
Getter Method
Signature
MaximumRadiusMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPolarRadiusModeTypes
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumRadiusMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderPolarRadiusModeTypes
) –New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MethodType¶
-
InspectionMethodBuilder.
MethodType
¶ Returns or sets the method feature type
-------------------------------------
Getter Method
Signature
MethodType
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderMethodTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MethodType
Parameters: type ( NXOpen.CAM.InspectionMethodBuilderMethodTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinSpacing¶
-
InspectionMethodBuilder.
MinSpacing
¶ Returns or sets the minimum spacing between scan points
-------------------------------------
Getter Method
Signature
MinSpacing
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinSpacing
Parameters: minSpacing (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinimumRadius¶
-
InspectionMethodBuilder.
MinimumRadius
¶ Returns or sets the minimum radius
-------------------------------------
Getter Method
Signature
MinimumRadius
Returns: Return type: float New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumRadius
Parameters: radius (float) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinimumRadiusMode¶
-
InspectionMethodBuilder.
MinimumRadiusMode
¶ Returns or sets the minimum radius mode
-------------------------------------
Getter Method
Signature
MinimumRadiusMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPolarRadiusModeTypes
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumRadiusMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderPolarRadiusModeTypes
) –New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NbScanPoints¶
-
InspectionMethodBuilder.
NbScanPoints
¶ Returns or sets the minimum number of scan points
-------------------------------------
Getter Method
Signature
NbScanPoints
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NbScanPoints
Parameters: count (int) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetDistance¶
-
InspectionMethodBuilder.
OffsetDistance
¶ Returns or sets the offset distance
-------------------------------------
Getter Method
Signature
OffsetDistance
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetDistance
Parameters: offsetDistance (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetEndAngle¶
-
InspectionMethodBuilder.
OffsetEndAngle
¶ Returns or sets the offset from end angle
-------------------------------------
Getter Method
Signature
OffsetEndAngle
Returns: Return type: float New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetEndAngle
Parameters: offsetAngle (float) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetMaximumRadius¶
-
InspectionMethodBuilder.
OffsetMaximumRadius
¶ Returns or sets the offset from maximum radius
-------------------------------------
Getter Method
Signature
OffsetMaximumRadius
Returns: Return type: float New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetMaximumRadius
Parameters: offset (float) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetMinimumRadius¶
-
InspectionMethodBuilder.
OffsetMinimumRadius
¶ Returns or sets the offset from minimum radius
-------------------------------------
Getter Method
Signature
OffsetMinimumRadius
Returns: Return type: float New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetMinimumRadius
Parameters: offset (float) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetStartAngle¶
-
InspectionMethodBuilder.
OffsetStartAngle
¶ Returns or sets the offset from start angle
-------------------------------------
Getter Method
Signature
OffsetStartAngle
Returns: Return type: float New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetStartAngle
Parameters: offsetAngle (float) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Pitch¶
-
InspectionMethodBuilder.
Pitch
¶ Returns or sets the pitch of the Scan Helix
-------------------------------------
Getter Method
Signature
Pitch
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Pitch
Parameters: pitch (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointCount¶
-
InspectionMethodBuilder.
PointCount
¶ Returns or sets the number of path points
-------------------------------------
Getter Method
Signature
PointCount
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointCount
Parameters: pointCount (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointHelix¶
-
InspectionMethodBuilder.
PointHelix
¶ Returns or sets a flag to indicate if point helix is allowed
-------------------------------------
Getter Method
Signature
PointHelix
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointHelix
Parameters: pointHelix (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceDirection¶
-
InspectionMethodBuilder.
PointSequenceDirection
¶ Returns or sets the point sequence start direction
-------------------------------------
Getter Method
Signature
PointSequenceDirection
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceDirectionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceDirection
Parameters: ptSeqDir ( NXOpen.CAM.InspectionMethodBuilderPointSequenceDirectionTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceMode¶
-
InspectionMethodBuilder.
PointSequenceMode
¶ Returns or sets the point sequence mode
-------------------------------------
Getter Method
Signature
PointSequenceMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceMode
Parameters: ptSeqMode ( NXOpen.CAM.InspectionMethodBuilderPointSequenceModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSequenceStart¶
-
InspectionMethodBuilder.
PointSequenceStart
¶ Returns or sets the point sequence start location
-------------------------------------
Getter Method
Signature
PointSequenceStart
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPointSequenceStartTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointSequenceStart
Parameters: ptSeqStart ( NXOpen.CAM.InspectionMethodBuilderPointSequenceStartTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PolarGrid¶
-
InspectionMethodBuilder.
PolarGrid
¶ Returns or sets a flag to indicate if circular point grid is allowed
-------------------------------------
Getter Method
Signature
PolarGrid
Returns: Return type: bool New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PolarGrid
Parameters: polarGrid (bool) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PolarPointSequence¶
-
InspectionMethodBuilder.
PolarPointSequence
¶ Returns or sets the polar point sequence mode
-------------------------------------
Getter Method
Signature
PolarPointSequence
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPolarPointSequenceTypes
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PolarPointSequence
Parameters: polSeqMode ( NXOpen.CAM.InspectionMethodBuilderPolarPointSequenceTypes
) –New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PolarSequenceDirection¶
-
InspectionMethodBuilder.
PolarSequenceDirection
¶ Returns or sets the polar sequence direction
-------------------------------------
Getter Method
Signature
PolarSequenceDirection
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPolarSequenceDirectionTypes
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PolarSequenceDirection
Parameters: polSeqDir ( NXOpen.CAM.InspectionMethodBuilderPolarSequenceDirectionTypes
) –New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PolarSequenceStart¶
-
InspectionMethodBuilder.
PolarSequenceStart
¶ Returns or sets the polar sequence start location
-------------------------------------
Getter Method
Signature
PolarSequenceStart
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderPolarSequenceStartTypes
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PolarSequenceStart
Parameters: polSeqStart ( NXOpen.CAM.InspectionMethodBuilderPolarSequenceStartTypes
) –New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProbeTipType¶
-
InspectionMethodBuilder.
ProbeTipType
¶ Returns or sets the preferred probe tip type
-------------------------------------
Getter Method
Signature
ProbeTipType
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderProbeTipTypes
New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProbeTipType
Parameters: tipType ( NXOpen.CAM.InspectionMoveBuilderProbeTipTypes
) –New in version NX9.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProfileDispositionMode¶
-
InspectionMethodBuilder.
ProfileDispositionMode
¶ Returns or sets the analysis profile disposition fitting mode
-------------------------------------
Getter Method
Signature
ProfileDispositionMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderProfileDispositionTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProfileDispositionMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderProfileDispositionTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RadialPointCount¶
-
InspectionMethodBuilder.
RadialPointCount
¶ Returns or sets the number of points in radial direction
-------------------------------------
Getter Method
Signature
RadialPointCount
Returns: Return type: int New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialPointCount
Parameters: ptCount (int) – New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReferenceFeatureMode¶
-
InspectionMethodBuilder.
ReferenceFeatureMode
¶ Returns or sets the relative measurement mode
-------------------------------------
Getter Method
Signature
ReferenceFeatureMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderReferenceFeatureModeTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeatureMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderReferenceFeatureModeTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReferenceFeatureOffsetDistance¶
-
InspectionMethodBuilder.
ReferenceFeatureOffsetDistance
¶ Returns or sets the offset distance for relative measurement
-------------------------------------
Getter Method
Signature
ReferenceFeatureOffsetDistance
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeatureOffsetDistance
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReferenceFeaturePointCount¶
-
InspectionMethodBuilder.
ReferenceFeaturePointCount
¶ Returns or sets the number of points for relative measurement
-------------------------------------
Getter Method
Signature
ReferenceFeaturePointCount
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeaturePointCount
Parameters: pointCount (int) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReferenceFeatureZoneRadius¶
-
InspectionMethodBuilder.
ReferenceFeatureZoneRadius
¶ Returns or sets the zone radius for relative measurement
-------------------------------------
Getter Method
Signature
ReferenceFeatureZoneRadius
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceFeatureZoneRadius
Parameters: radius (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RetractDistance¶
-
InspectionMethodBuilder.
RetractDistance
¶ Returns or sets the retract distance
-------------------------------------
Getter Method
Signature
RetractDistance
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RetractDistance
Parameters: distance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Revolutions¶
-
InspectionMethodBuilder.
Revolutions
¶ Returns or sets the revolutions of the Scan Helix
-------------------------------------
Getter Method
Signature
Revolutions
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Revolutions
Parameters: revolutions (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanCurveMode¶
-
InspectionMethodBuilder.
ScanCurveMode
¶ Returns or sets the scan curve mode
-------------------------------------
Getter Method
Signature
ScanCurveMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanCurveModeTypes
New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanCurveMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderScanCurveModeTypes
) –New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanForce¶
-
InspectionMethodBuilder.
ScanForce
¶ Returns or sets the scan force
-------------------------------------
Getter Method
Signature
ScanForce
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanForce
Parameters: force (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanModeType¶
-
InspectionMethodBuilder.
ScanModeType
¶ Returns or sets the 3,5 axis scan mode type
-------------------------------------
Getter Method
Signature
ScanModeType
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanModeTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanModeType
Parameters: modeType ( NXOpen.CAM.InspectionMethodBuilderScanModeTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScanSpeed¶
-
InspectionMethodBuilder.
ScanSpeed
¶ Returns or sets the scan speed
-------------------------------------
Getter Method
Signature
ScanSpeed
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScanSpeed
Parameters: speed (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorStrategy¶
-
InspectionMethodBuilder.
SensorStrategy
¶ Returns or sets the sensor selection strategy
-------------------------------------
Getter Method
Signature
SensorStrategy
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderSensorStrategyTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorStrategy
Parameters: sensorStrategy ( NXOpen.CAM.InspectionMoveBuilderSensorStrategyTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Speed¶
-
InspectionMethodBuilder.
Speed
¶ Returns or sets the default animation speed setting
-------------------------------------
Getter Method
Signature
Speed
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Speed
Parameters: speed (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartDistance¶
-
InspectionMethodBuilder.
StartDistance
¶ Returns or sets the start point offset distance along the scan
-------------------------------------
Getter Method
Signature
StartDistance
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartDistance
Parameters: startDistance (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartEndMode¶
-
InspectionMethodBuilder.
StartEndMode
¶ Returns or sets the scan start end mode
-------------------------------------
Getter Method
Signature
StartEndMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartEndMode
Parameters: startEndMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartPercentage¶
-
InspectionMethodBuilder.
StartPercentage
¶ Returns or sets the start percentage along the scan
-------------------------------------
Getter Method
Signature
StartPercentage
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPercentage
Parameters: startPercentage (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StepSize¶
-
InspectionMethodBuilder.
StepSize
¶ Returns or sets the scan step size
-------------------------------------
Getter Method
Signature
StepSize
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StepSize
Parameters: step (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StopRadius¶
-
InspectionMethodBuilder.
StopRadius
¶ Returns or sets the scan stop radius
-------------------------------------
Getter Method
Signature
StopRadius
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StopRadius
Parameters: radius (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SurfaceProfileMode¶
-
InspectionMethodBuilder.
SurfaceProfileMode
¶ Returns or sets the analysis surface profile fitting mode
-------------------------------------
Getter Method
Signature
SurfaceProfileMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderSurfaceProfileTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceProfileMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderSurfaceProfileTypes
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Sweep¶
-
InspectionMethodBuilder.
Sweep
¶ Returns or sets the sweep of the Scan Helix
-------------------------------------
Getter Method
Signature
Sweep
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sweep
Parameters: sweep (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TiltAngle¶
-
InspectionMethodBuilder.
TiltAngle
¶ Returns or sets the tilt angle (degrees)
-------------------------------------
Getter Method
Signature
TiltAngle
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TiltAngle
Parameters: angle (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TurnDirection¶
-
InspectionMethodBuilder.
TurnDirection
¶ Returns or sets the turn direction type of the Scan Helix
-------------------------------------
Getter Method
Signature
TurnDirection
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanHelixTurnDirectionTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TurnDirection
Parameters: turnDirection ( NXOpen.CAM.InspectionMethodBuilderScanHelixTurnDirectionTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TurnType¶
-
InspectionMethodBuilder.
TurnType
¶ Returns or sets the turn type of the Scan Helix
-------------------------------------
Getter Method
Signature
TurnType
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanHelixTurnTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TurnType
Parameters: turnType ( NXOpen.CAM.InspectionMethodBuilderScanHelixTurnTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UCount¶
-
InspectionMethodBuilder.
UCount
¶ Returns or sets the number of points in U direction
-------------------------------------
Getter Method
Signature
UCount
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UCount
Parameters: uCount (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEnd¶
-
InspectionMethodBuilder.
UEnd
¶ Returns or sets the U end parameter
-------------------------------------
Getter Method
Signature
UEnd
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEnd
Parameters: uEnd (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEndDeg¶
-
InspectionMethodBuilder.
UEndDeg
¶ Returns or sets the U end degrees
-------------------------------------
Getter Method
Signature
UEndDeg
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEndDeg
Parameters: uEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEndDist¶
-
InspectionMethodBuilder.
UEndDist
¶ Returns or sets the U end distance
-------------------------------------
Getter Method
Signature
UEndDist
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEndDist
Parameters: uEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEndMode¶
-
InspectionMethodBuilder.
UEndMode
¶ Returns or sets the end U mode
-------------------------------------
Getter Method
Signature
UEndMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEndMode
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UEndSweep¶
-
InspectionMethodBuilder.
UEndSweep
¶ Returns or sets the U sweep degrees
-------------------------------------
Getter Method
Signature
UEndSweep
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UEndSweep
Parameters: uEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStart¶
-
InspectionMethodBuilder.
UStart
¶ Returns or sets the U start parameter
-------------------------------------
Getter Method
Signature
UStart
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStart
Parameters: uStart (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStartDeg¶
-
InspectionMethodBuilder.
UStartDeg
¶ Returns or sets the U start degrees
-------------------------------------
Getter Method
Signature
UStartDeg
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStartDeg
Parameters: uStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStartDist¶
-
InspectionMethodBuilder.
UStartDist
¶ Returns or sets the U start distance
-------------------------------------
Getter Method
Signature
UStartDist
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStartDist
Parameters: uStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStartMode¶
-
InspectionMethodBuilder.
UStartMode
¶ Returns or sets the start U mode
-------------------------------------
Getter Method
Signature
UStartMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStartMode
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UStartSweep¶
-
InspectionMethodBuilder.
UStartSweep
¶ Returns or sets the U start sweep degrees
-------------------------------------
Getter Method
Signature
UStartSweep
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UStartSweep
Parameters: uStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UVGrid¶
-
InspectionMethodBuilder.
UVGrid
¶ Returns or sets a flag to indicate if rectangular UV grid is allowed
-------------------------------------
Getter Method
Signature
UVGrid
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UVGrid
Parameters: uvGrid (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VCount¶
-
InspectionMethodBuilder.
VCount
¶ Returns or sets the number of points in V direction
-------------------------------------
Getter Method
Signature
VCount
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VCount
Parameters: vCount (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEnd¶
-
InspectionMethodBuilder.
VEnd
¶ Returns or sets the V end parameter
-------------------------------------
Getter Method
Signature
VEnd
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEnd
Parameters: vEnd (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEndDeg¶
-
InspectionMethodBuilder.
VEndDeg
¶ Returns or sets the V end degrees
-------------------------------------
Getter Method
Signature
VEndDeg
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEndDeg
Parameters: vEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEndDist¶
-
InspectionMethodBuilder.
VEndDist
¶ Returns or sets the V end distance
-------------------------------------
Getter Method
Signature
VEndDist
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEndDist
Parameters: vEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEndMode¶
-
InspectionMethodBuilder.
VEndMode
¶ Returns or sets the end V mode
-------------------------------------
Getter Method
Signature
VEndMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEndMode
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VEndSweep¶
-
InspectionMethodBuilder.
VEndSweep
¶ Returns or sets the V sweep degrees
-------------------------------------
Getter Method
Signature
VEndSweep
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VEndSweep
Parameters: vEnd (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStart¶
-
InspectionMethodBuilder.
VStart
¶ Returns or sets the V start parameter
-------------------------------------
Getter Method
Signature
VStart
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStart
Parameters: vStart (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStartDeg¶
-
InspectionMethodBuilder.
VStartDeg
¶ Returns or sets the V start degrees
-------------------------------------
Getter Method
Signature
VStartDeg
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStartDeg
Parameters: vStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStartDist¶
-
InspectionMethodBuilder.
VStartDist
¶ Returns or sets the V start distance
-------------------------------------
Getter Method
Signature
VStartDist
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStartDist
Parameters: vStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStartMode¶
-
InspectionMethodBuilder.
VStartMode
¶ Returns or sets the start V mode
-------------------------------------
Getter Method
Signature
VStartMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStartMode
Parameters: uvMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VStartSweep¶
-
InspectionMethodBuilder.
VStartSweep
¶ Returns or sets the V start sweep degrees
-------------------------------------
Getter Method
Signature
VStartSweep
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VStartSweep
Parameters: vStart (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
InspectionMethodBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.