InspectionMethodBuilderOperationTypes Enumeration¶
NXOpen.CAM.InspectionMethodBuilder.OperationTypes is an alias for NXOpen.CAM.InspectionMethodBuilderOperationTypes
-
class
NXOpen.CAM.
InspectionMethodBuilderOperationTypes
¶ Bases:
object
CMM Inspection operation types.
Enum Members
Enum Member Enum Member Description NotSet None ManualPoint Measured Point UVGrid Point Set (Rectangular UV Grid) PointHelix Point Helix LineScan Scan Line CircularScan Scan Arc CurveScan Scan Curve HelicalScan Scan Helix CurveScan5axis 5-axis Scan Curve LinearSafeMoveToPoint Linear Safe Move To Point DeltaMove Delta Move Linear5axisMoveToPoint Linear 5-axis Move To Point PolarGrid Circular Point Set (Polar Grid) -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-