NCGroupBuilder Class¶
-
class
NXOpen.CAM.
NCGroupBuilder
¶ Bases:
NXOpen.CAM.ParamBuilder
Represents a NCGroup Builder
This is an abstract class, and cannot be instantiated.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
OptimizationMethod | Returns or sets the optim method |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Description¶
-
NCGroupBuilder.
Description
¶ Returns or sets the description
-------------------------------------
Getter Method
Signature
Description
Returns: the description Return type: str New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
Description
Parameters: description (str) – the description New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
EndUdeSet¶
-
NCGroupBuilder.
EndUdeSet
¶ Returns the end ude set
-------------------------------------
Getter Method
Signature
EndUdeSet
Returns: the end ude set Return type: NXOpen.CAM.UdeSet
New in version NX7.5.0.
License requirements: None.
StartUdeSet¶
-
NCGroupBuilder.
StartUdeSet
¶ Returns the start ude set
-------------------------------------
Getter Method
Signature
StartUdeSet
Returns: the start ude set Return type: NXOpen.CAM.UdeSet
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
NCGroupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.