UdeSet Class¶
-
class
NXOpen.CAM.
UdeSet
¶ Bases:
NXOpen.TaggedObject
Represets a set of User Defined Events
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateUde | Sets the creator for Ude |
CreateUdeByName | The function to add Ude |
Property Detail¶
UdeList¶
-
UdeSet.
UdeList
¶ Returns the Ude List
-------------------------------------
Getter Method
Signature
UdeList
Returns: the list of udes Return type: NXOpen.CAM.UdeList
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
CreateUde¶
-
UdeSet.
CreateUde
¶ Sets the creator for Ude
Signature
CreateUde()
Returns: the Ude object Return type: NXOpen.CAM.Ude
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CreateUdeByName¶
-
UdeSet.
CreateUdeByName
¶ The function to add Ude
Signature
CreateUdeByName(udeName)
Parameters: udeName (str) – The UDE name Returns: the Ude object Return type: NXOpen.CAM.Ude
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)