Ude Class¶
-
class
NXOpen.CAM.
Ude
¶ Bases:
NXOpen.TaggedObject
Represets a User Defined Event
To create a new instance of this class, use
NXOpen.CAM.UdeSet.CreateUde()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
NumberOfParameters | Returns the number of parameters |
OutputLoadTool | Returns or sets the output load tool |
Tag | Returns the Tag for this object. |
UdeName | Returns or sets the ude name |
Methods¶
Method | Description |
---|---|
GetParameter | Get the parameter for the specified parameter name |
GetParameterNames | Returns the parameter names |
Property Detail¶
NumberOfParameters¶
-
Ude.
NumberOfParameters
¶ Returns the number of parameters
-------------------------------------
Getter Method
Signature
NumberOfParameters
Returns: the number of parameters Return type: int New in version NX7.5.0.
License requirements: None.
OutputLoadTool¶
-
Ude.
OutputLoadTool
¶ Returns or sets the output load tool
-------------------------------------
Getter Method
Signature
OutputLoadTool
Returns: if output load tool Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputLoadTool
Parameters: loadTool (bool) – output load tool New in version NX7.5.0.
License requirements: None.
UdeName¶
-
Ude.
UdeName
¶ Returns or sets the ude name
-------------------------------------
Getter Method
Signature
UdeName
Returns: the name of the ude Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UdeName
Parameters: udeName (str) – the name of the Ude New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetParameter¶
-
Ude.
GetParameter
¶ Overloaded method GetParameter
GetParameter(parameterName)
GetParameter(index)
-------------------------------------
Get the parameter for the specified parameter name
Signature
GetParameter(parameterName)
Parameters: parameterName (str) – the parameter name Returns: the parameter Return type: NXOpen.CAM.UdeParameter
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Get the parameter for the specified index
Signature
GetParameter(index)
Parameters: index (int) – the parameter index Returns: the parameter Return type: NXOpen.CAM.UdeParameter
New in version NX8.0.0.
License requirements: None.
-------------------------------------