InspectionMethodBuilderMethodTypes Enumeration¶
NXOpen.CAM.InspectionMethodBuilder.MethodTypes is an alias for NXOpen.CAM.InspectionMethodBuilderMethodTypes
-
class
NXOpen.CAM.
InspectionMethodBuilderMethodTypes
¶ Bases:
object
CMM Inspection method feature type.
Enum Members
Enum Member Enum Member Description NotSet None Arc Arc Circle Circle Point Point Sphere Sphere Surface Surface Pattern Pattern Curve Curve Cylinder Cylinder Cone Cone Plane Plane Line Line CParln Bounded Slot Tab SlotTab Slot Tab SurfaceOfRevolution Surface of Revolution Torus Torus EdgePt Edge Point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-