InspectionMethodBuilderScanModeTypes Enumeration¶
NXOpen.CAM.InspectionMethodBuilder.ScanModeTypes is an alias for NXOpen.CAM.InspectionMethodBuilderScanModeTypes
-
class
NXOpen.CAM.
InspectionMethodBuilderScanModeTypes
¶ Bases:
object
the scan mode 3-axis, 5-axis type
Enum Members
Enum Member Enum Member Description Mode3axis 3-axis mode Mode5axis 5-axis mode -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-