InspectionMethodBuilderPolarSequenceStartTypes Enumeration¶
NXOpen.CAM.InspectionMethodBuilder.PolarSequenceStartTypes is an alias for NXOpen.CAM.InspectionMethodBuilderPolarSequenceStartTypes
-
class
NXOpen.CAM.
InspectionMethodBuilderPolarSequenceStartTypes
¶ Bases:
object
the polar sequence start mode
Enum Members
Enum Member Enum Member Description RminAmin min Radius - min Angle RminAmax min Radius - max Angle RmaxAmin max Radius - min Angle RmaxAmax max Radius - max Angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-