InspectionMethodBuilderUVModeTypes Enumeration¶
NXOpen.CAM.InspectionMethodBuilder.UVModeTypes is an alias for NXOpen.CAM.InspectionMethodBuilderUVModeTypes
-
class
NXOpen.CAM.
InspectionMethodBuilderUVModeTypes
¶ Bases:
object
the UV modes
Enum Members
Enum Member Enum Member Description Percentage Percentage Distance Distance from start and end in part units Full Full circumference Degrees Angle from start and end Sweep Start angle and sweep angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-