InspectionMethodBuilderPointSequenceDirectionTypes Enumeration¶
NXOpen.CAM.InspectionMethodBuilder.PointSequenceDirectionTypes is an alias for NXOpen.CAM.InspectionMethodBuilderPointSequenceDirectionTypes
-
class
NXOpen.CAM.
InspectionMethodBuilderPointSequenceDirectionTypes
¶ Bases:
object
the point sequence start direction
Enum Members
Enum Member Enum Member Description U Order by U V Order by V -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-