NXOpen.Validate Package¶
Classes¶
CheckerNode Class | Represents a checker that validator will use to check against part node. |
Override Class | Represents a NXOpen.Validate.Override object. |
OverrideBuilder Class | Represents a NXOpen.Validate.Override builder |
Parser Class | Represents a NX NXOpen.Validate.Parser . |
PartNode Class | Represents a part file that validator will check against. |
Requirement Class | Represents a NXOpen.Validate.Requirement object. |
RequirementBuilder Class | Represents a NXOpen.Validate.Requirement builder |
RequirementCheck Class | Represents an NX NXOpen.Validate.RequirementCheck object. |
RequirementCheckCollection Class | Represents an NX NXOpen.Validate.RequirementCheckCollection object. |
RequirementCollection Class | Represents an NX NXOpen.Validate.RequirementCollection object. |
ResultObject Class |
|
ValidationManager Class | Represents an object that manages validator and parser associated instance objects. |
Validator Class | Represents a NX NXOpen.Validate.Validator . |
ValidatorOptions Class | Contains information about run options of check-mate checking process. |
XmlComparator Class | Provides a generic comparator for finding differences between two XML format files. The comparator takes NXOpen.Validate.XmlComparatorOptions_Struct to further control the comparison process. It returns NXOpen.Validate.XmlComparatorResult , and generates report of detailed differences in HTML file which can be viewed via web browser. |
Enumerations¶
OverrideBuilderDecisionActions Enumeration | Represents the override request decision action |
OverrideBuilderRequestTypes Enumeration | Represents the override request type |
OverrideBuilderToStates Enumeration | Represents the override request to state |
ParserDataSourceTypes Enumeration | The data source type of check result. |
RequirementBuilderDataTypeOptions Enumeration | This enum represents the data type of the value in requirement |
RequirementBuilderDefinitionMethodOptions Enumeration | This enum represents the type of requirement definition method |
RequirementBuilderRelationalOperatorOptions Enumeration | This enum represents the relational operator for comparing values |
RequirementBuilderSeverityOptions Enumeration | This enum represents the severity level when a requirement is not satisfied |
RequirementCheckSaveResultsToTeamcenterOptions Enumeration | This enum represents the Save Results to Teamcenter option |
RequirementCollectionSourceTypeOptions Enumeration | This enum represents the type of external source where requirement is defined |
ResultObjectResultTypes Enumeration | The type of check result |
ValidatorOptionsLogModeTypes Enumeration | The log mode type. |
ValidatorOptionsResultsDisplayModeTypes Enumeration | The results display mode type. |
ValidatorOptionsSaveModeTypes Enumeration | The save mode type. |
XmlComparatorResult Enumeration | Specifies result of the comparison |
Structs¶
XmlComparatorOptions_Struct Struct | <para>Represents config options in comparison</para> <para>For example:</para> <para>case 1: Defines filter file to control what nodes will be compared; generates comparison report and log; ignores CDATA and processing instruction nodes. |