XmlComparatorResult Enumeration

NXOpen.Validate.XmlComparator.Result is an alias for NXOpen.Validate.XmlComparatorResult

class NXOpen.Validate.XmlComparatorResult

Bases: object

Specifies result of the comparison

Enum Members

Enum Member Enum Member Description
Identical
Represents two xml files are identical
Different
Represents two xml files are different
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.