RequirementCheckSaveResultsToTeamcenterOptions Enumeration¶
NXOpen.Validate.RequirementCheck.SaveResultsToTeamcenterOptions is an alias for NXOpen.Validate.RequirementCheckSaveResultsToTeamcenterOptions
-
class
NXOpen.Validate.
RequirementCheckSaveResultsToTeamcenterOptions
¶ Bases:
object
This enum represents the Save Results to Teamcenter option
Enum Members
Enum Member Enum Member Description DoNotSave Do not perform save.SaveIfPassed Perform save only if the result is passed.AlwaysSave Always perform save-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-