ValidatorOptionsLogModeTypes Enumeration

NXOpen.Validate.ValidatorOptions.LogModeTypes is an alias for NXOpen.Validate.ValidatorOptionsLogModeTypes

class NXOpen.Validate.ValidatorOptionsLogModeTypes

Bases: object

The log mode type.

Enum Members

Enum Member Enum Member Description
LogPerSession
Generate log per session
LogPerPart
Generate log per part
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.