ParserDataSourceTypes Enumeration

NXOpen.Validate.Parser.DataSourceTypes is an alias for NXOpen.Validate.ParserDataSourceTypes

class NXOpen.Validate.ParserDataSourceTypes

Bases: object

The data source type of check result.

Enum Members

Enum Member Enum Member Description
MostRecentRun
Result of most recent run
ResultFromPart
Result from part
ResultFromTeamcenter
Result from Teamcenter
ResultFromNXChecks
Result from NX checks
ResultFromLogFile
Result from Log File
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.