RequirementCollectionSourceTypeOptions Enumeration

NXOpen.Validate.RequirementCollection.SourceTypeOptions is an alias for NXOpen.Validate.RequirementCollectionSourceTypeOptions

class NXOpen.Validate.RequirementCollectionSourceTypeOptions

Bases: object

This enum represents the type of external source where requirement is defined

Enum Members

Enum Member Enum Member Description
LocalFile
TeamcenterFile
Teamcenter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.