ValidatorOptionsSaveModeTypes Enumeration

NXOpen.Validate.ValidatorOptions.SaveModeTypes is an alias for NXOpen.Validate.ValidatorOptionsSaveModeTypes

class NXOpen.Validate.ValidatorOptionsSaveModeTypes

Bases: object

The save mode type.

Enum Members

Enum Member Enum Member Description
DoNotSave
Do not perform save.
SaveIfPassed
Perform save only if the checking is passed.
AlwaysSave
Always perform save
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.