ValidatorOptionsResultsDisplayModeTypes Enumeration

NXOpen.Validate.ValidatorOptions.ResultsDisplayModeTypes is an alias for NXOpen.Validate.ValidatorOptionsResultsDisplayModeTypes

class NXOpen.Validate.ValidatorOptionsResultsDisplayModeTypes

Bases: object

The results display mode type.

Enum Members

Enum Member Enum Member Description
AlwaysDisplay
Always display results.
DisplayIfNotPass
Display results if the checking is not passed.
DoNotDisplay
Do not display results
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.