InspectionCmmCommandBuilder Class¶
-
class
NXOpen.CAM.
InspectionCmmCommandBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection miscellaneous command builder.
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionCmmCommandBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AngularPlaces | Returns or sets the angular decimal places |
AngularUnits | Returns or sets the angular units |
AutoToggle | Returns or sets the auto mode toggle |
ChannelName | Returns or sets the channel’s name |
CommandType | Returns or sets the command type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
DevTolPlaces | Returns or sets the deviation and tolerance decimal places |
DeviceName | Returns or sets the device name |
DeviceType | Returns or sets the device type |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GotoAangle | Returns or sets the goto A angle |
GotoBangle | Returns or sets the goto B angle |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
HomePtMethod | Returns or sets the home point method |
HomePtPoint | Returns or sets the home point location |
HumidityPlaces | Returns or sets the humidity decimal places |
IdName | Returns or sets the ID name |
IdnameMethod | Returns or sets the ID name method |
IndexSize | Returns or sets the index size |
IntermediatePoint | Returns or sets the intermediate point |
JumpLabel | Returns or sets the program jump label |
LayoutAndLayer | Returns the Layer and Layout |
LinearPlaces | Returns or sets the linear decimal places |
LinearUnits | Returns or sets the linear units |
ManualToggle | Returns or sets the manual mode toggle |
MaxToggle | Returns or sets the max toggle |
MaxValue | Returns or sets the max value |
MinToggle | Returns or sets the min toggle |
MinValue | Returns or sets the min value |
MotionOutputBuilder | Returns the motion output builder |
MoveType | Returns or sets the move type |
Notes | Returns the notes builder |
NumChar | Returns or sets the number of characters |
OpName | Returns or sets the command operation name |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ProgramName | Returns or sets the program name |
ProgramNameMethod | Returns or sets the program name method |
ProgramToggle | Returns or sets the program mode toggle |
PromptVar | Returns or sets the prompt variable |
QisvarType | Returns or sets the qis variable type |
QisvarValue | Returns or sets the qis variable value |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
RevMethod | Returns or sets the revision method |
RevName | Returns or sets the revision name |
SafeClearance | Returns the safe clearance builder |
SaveDmlDidLabel | Returns or sets the save DML DID label |
SaveDmlPcsLabel | Returns or sets the save DML PCS label |
SaveDmlPointData | Returns or sets the save DML point data |
SaveDmlVersion | Returns or sets the save DML version |
SelectToolFlag | Returns or sets the user selected tool |
SensorName | Returns or sets the sensor name |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TargetPoint | Returns or sets the target point |
TemperaturePlaces | Returns or sets the temperature decimal places |
TemperatureUnits | Returns or sets the temperature units |
ToolChangeSetting | Returns the tool change builder |
ToolName | Returns or sets the tool name |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
UserPrompt | Returns or sets the user prompt |
VarName | Returns or sets the variable name |
VarScope | Returns or sets the variable scope |
VarType | Returns or sets the variable type |
VectorPlaces | Returns or sets the vector decimal places |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
GetProgStatements | Returns the program statements @return |
SetHoleAxisValues | Set the Hole Axis values |
SetProgStatements | Sets the program statements |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AngularPlaces¶
-
InspectionCmmCommandBuilder.
AngularPlaces
¶ Returns or sets the angular decimal places
-------------------------------------
Getter Method
Signature
AngularPlaces()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularPlaces(angularPlaces)
Parameters: angularPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AngularUnits¶
-
InspectionCmmCommandBuilder.
AngularUnits
¶ Returns or sets the angular units
-------------------------------------
Getter Method
Signature
AngularUnits()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderAngularUnitsOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularUnits(angularUnits)
Parameters: angularUnits ( NXOpen.CAM.InspectionCmmCommandBuilderAngularUnitsOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AutoToggle¶
-
InspectionCmmCommandBuilder.
AutoToggle
¶ Returns or sets the auto mode toggle
-------------------------------------
Getter Method
Signature
AutoToggle()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoToggle(autoToggle)
Parameters: autoToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CommandType¶
-
InspectionCmmCommandBuilder.
CommandType
¶ Returns or sets the command type
-------------------------------------
Getter Method
Signature
CommandType()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderCommandTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CommandType(commandType)
Parameters: commandType ( NXOpen.CAM.InspectionCmmCommandBuilderCommandTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DevTolPlaces¶
-
InspectionCmmCommandBuilder.
DevTolPlaces
¶ Returns or sets the deviation and tolerance decimal places
-------------------------------------
Getter Method
Signature
DevTolPlaces()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DevTolPlaces(devTolPlaces)
Parameters: devTolPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DeviceName¶
-
InspectionCmmCommandBuilder.
DeviceName
¶ Returns or sets the device name
-------------------------------------
Getter Method
Signature
DeviceName()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeviceName(deviceName)
Parameters: deviceName (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DeviceType¶
-
InspectionCmmCommandBuilder.
DeviceType
¶ Returns or sets the device type
-------------------------------------
Getter Method
Signature
DeviceType()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderDeviceTypeOptions
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeviceType(deviceType)
Parameters: deviceType ( NXOpen.CAM.InspectionCmmCommandBuilderDeviceTypeOptions
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
GotoAangle¶
-
InspectionCmmCommandBuilder.
GotoAangle
¶ Returns or sets the goto A angle
-------------------------------------
Getter Method
Signature
GotoAangle()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GotoAangle(gotoAangle)
Parameters: gotoAangle (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
GotoBangle¶
-
InspectionCmmCommandBuilder.
GotoBangle
¶ Returns or sets the goto B angle
-------------------------------------
Getter Method
Signature
GotoBangle()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GotoBangle(gotoBangle)
Parameters: gotoBangle (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
HomePtMethod¶
-
InspectionCmmCommandBuilder.
HomePtMethod
¶ Returns or sets the home point method
-------------------------------------
Getter Method
Signature
HomePtMethod()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderHomePtMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HomePtMethod(homePtMethod)
Parameters: homePtMethod ( NXOpen.CAM.InspectionCmmCommandBuilderHomePtMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
HomePtPoint¶
-
InspectionCmmCommandBuilder.
HomePtPoint
¶ Returns or sets the home point location
-------------------------------------
Getter Method
Signature
HomePtPoint()
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HomePtPoint(homePtPoint)
Parameters: homePtPoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
HumidityPlaces¶
-
InspectionCmmCommandBuilder.
HumidityPlaces
¶ Returns or sets the humidity decimal places
-------------------------------------
Getter Method
Signature
HumidityPlaces()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HumidityPlaces(humidityPlaces)
Parameters: humidityPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IdName¶
-
InspectionCmmCommandBuilder.
IdName
¶ Returns or sets the ID name
-------------------------------------
Getter Method
Signature
IdName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdName(idName)
Parameters: idName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IdnameMethod¶
-
InspectionCmmCommandBuilder.
IdnameMethod
¶ Returns or sets the ID name method
-------------------------------------
Getter Method
Signature
IdnameMethod()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderIdnameMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdnameMethod(idnameMethod)
Parameters: idnameMethod ( NXOpen.CAM.InspectionCmmCommandBuilderIdnameMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IndexSize¶
-
InspectionCmmCommandBuilder.
IndexSize
¶ Returns or sets the index size
-------------------------------------
Getter Method
Signature
IndexSize()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndexSize(indexSize)
Parameters: indexSize (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IntermediatePoint¶
-
InspectionCmmCommandBuilder.
IntermediatePoint
¶ Returns or sets the intermediate point
-------------------------------------
Getter Method
Signature
IntermediatePoint()
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediatePoint(intermediatePoint)
Parameters: intermediatePoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
JumpLabel¶
-
InspectionCmmCommandBuilder.
JumpLabel
¶ Returns or sets the program jump label
-------------------------------------
Getter Method
Signature
JumpLabel()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JumpLabel(jumpLabel)
Parameters: jumpLabel (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LinearPlaces¶
-
InspectionCmmCommandBuilder.
LinearPlaces
¶ Returns or sets the linear decimal places
-------------------------------------
Getter Method
Signature
LinearPlaces()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearPlaces(linearPlaces)
Parameters: linearPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LinearUnits¶
-
InspectionCmmCommandBuilder.
LinearUnits
¶ Returns or sets the linear units
-------------------------------------
Getter Method
Signature
LinearUnits()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderLinearUnitsOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearUnits(linearUnits)
Parameters: linearUnits ( NXOpen.CAM.InspectionCmmCommandBuilderLinearUnitsOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ManualToggle¶
-
InspectionCmmCommandBuilder.
ManualToggle
¶ Returns or sets the manual mode toggle
-------------------------------------
Getter Method
Signature
ManualToggle()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ManualToggle(manualToggle)
Parameters: manualToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaxToggle¶
-
InspectionCmmCommandBuilder.
MaxToggle
¶ Returns or sets the max toggle
-------------------------------------
Getter Method
Signature
MaxToggle()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxToggle(maxToggle)
Parameters: maxToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaxValue¶
-
InspectionCmmCommandBuilder.
MaxValue
¶ Returns or sets the max value
-------------------------------------
Getter Method
Signature
MaxValue()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxValue(maxValue)
Parameters: maxValue (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinToggle¶
-
InspectionCmmCommandBuilder.
MinToggle
¶ Returns or sets the min toggle
-------------------------------------
Getter Method
Signature
MinToggle()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinToggle(minToggle)
Parameters: minToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinValue¶
-
InspectionCmmCommandBuilder.
MinValue
¶ Returns or sets the min value
-------------------------------------
Getter Method
Signature
MinValue()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinValue(minValue)
Parameters: minValue (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MoveType¶
-
InspectionCmmCommandBuilder.
MoveType
¶ Returns or sets the move type
-------------------------------------
Getter Method
Signature
MoveType()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderMoveTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MoveType(moveType)
Parameters: moveType ( NXOpen.CAM.InspectionCmmCommandBuilderMoveTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NumChar¶
-
InspectionCmmCommandBuilder.
NumChar
¶ Returns or sets the number of characters
-------------------------------------
Getter Method
Signature
NumChar()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumChar(numChar)
Parameters: numChar (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OpName¶
-
InspectionCmmCommandBuilder.
OpName
¶ Returns or sets the command operation name
-------------------------------------
Getter Method
Signature
OpName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OpName(opName)
Parameters: opName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProgramName¶
-
InspectionCmmCommandBuilder.
ProgramName
¶ Returns or sets the program name
-------------------------------------
Getter Method
Signature
ProgramName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramName(programName)
Parameters: programName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProgramNameMethod¶
-
InspectionCmmCommandBuilder.
ProgramNameMethod
¶ Returns or sets the program name method
-------------------------------------
Getter Method
Signature
ProgramNameMethod()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderProgramNameMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramNameMethod(programNameMethod)
Parameters: programNameMethod ( NXOpen.CAM.InspectionCmmCommandBuilderProgramNameMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProgramToggle¶
-
InspectionCmmCommandBuilder.
ProgramToggle
¶ Returns or sets the program mode toggle
-------------------------------------
Getter Method
Signature
ProgramToggle()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramToggle(programToggle)
Parameters: programToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PromptVar¶
-
InspectionCmmCommandBuilder.
PromptVar
¶ Returns or sets the prompt variable
-------------------------------------
Getter Method
Signature
PromptVar()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderPromptVars
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PromptVar(promptVar)
Parameters: promptVar ( NXOpen.CAM.InspectionCmmCommandBuilderPromptVars
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
QisvarType¶
-
InspectionCmmCommandBuilder.
QisvarType
¶ Returns or sets the qis variable type
-------------------------------------
Getter Method
Signature
QisvarType()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderQisvarTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
QisvarType(qisvarType)
Parameters: qisvarType ( NXOpen.CAM.InspectionCmmCommandBuilderQisvarTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
QisvarValue¶
-
InspectionCmmCommandBuilder.
QisvarValue
¶ Returns or sets the qis variable value
-------------------------------------
Getter Method
Signature
QisvarValue()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
QisvarValue(qisvarValue)
Parameters: qisvarValue (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RevMethod¶
-
InspectionCmmCommandBuilder.
RevMethod
¶ Returns or sets the revision method
-------------------------------------
Getter Method
Signature
RevMethod()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderRevMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RevMethod(revMethod)
Parameters: revMethod ( NXOpen.CAM.InspectionCmmCommandBuilderRevMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RevName¶
-
InspectionCmmCommandBuilder.
RevName
¶ Returns or sets the revision name
-------------------------------------
Getter Method
Signature
RevName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RevName(revName)
Parameters: revName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDmlDidLabel¶
-
InspectionCmmCommandBuilder.
SaveDmlDidLabel
¶ Returns or sets the save DML DID label
-------------------------------------
Getter Method
Signature
SaveDmlDidLabel()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDmlDidLabel(saveDmlDidLabel)
Parameters: saveDmlDidLabel (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDmlPcsLabel¶
-
InspectionCmmCommandBuilder.
SaveDmlPcsLabel
¶ Returns or sets the save DML PCS label
-------------------------------------
Getter Method
Signature
SaveDmlPcsLabel()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDmlPcsLabel(savePcsDidLabel)
Parameters: savePcsDidLabel (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDmlPointData¶
-
InspectionCmmCommandBuilder.
SaveDmlPointData
¶ Returns or sets the save DML point data
-------------------------------------
Getter Method
Signature
SaveDmlPointData()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDmlPointData(saveDmlPointData)
Parameters: saveDmlPointData (bool) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDmlVersion¶
-
InspectionCmmCommandBuilder.
SaveDmlVersion
¶ Returns or sets the save DML version
-------------------------------------
Getter Method
Signature
SaveDmlVersion()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDmlVersion(saveDmlVersion)
Parameters: saveDmlVersion (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorName¶
-
InspectionCmmCommandBuilder.
SensorName
¶ Returns or sets the sensor name
-------------------------------------
Getter Method
Signature
SensorName()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorName(sensorName)
Parameters: sensorName (str) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TargetPoint¶
-
InspectionCmmCommandBuilder.
TargetPoint
¶ Returns or sets the target point
-------------------------------------
Getter Method
Signature
TargetPoint()
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetPoint(targetPoint)
Parameters: targetPoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TemperaturePlaces¶
-
InspectionCmmCommandBuilder.
TemperaturePlaces
¶ Returns or sets the temperature decimal places
-------------------------------------
Getter Method
Signature
TemperaturePlaces()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemperaturePlaces(temperaturePlaces)
Parameters: temperaturePlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TemperatureUnits¶
-
InspectionCmmCommandBuilder.
TemperatureUnits
¶ Returns or sets the temperature units
-------------------------------------
Getter Method
Signature
TemperatureUnits()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderTemperatureUnitsOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemperatureUnits(temperatureUnits)
Parameters: temperatureUnits ( NXOpen.CAM.InspectionCmmCommandBuilderTemperatureUnitsOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ToolName¶
-
InspectionCmmCommandBuilder.
ToolName
¶ Returns or sets the tool name
-------------------------------------
Getter Method
Signature
ToolName()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolName(toolName)
Parameters: toolName (str) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UserPrompt¶
-
InspectionCmmCommandBuilder.
UserPrompt
¶ Returns or sets the user prompt
-------------------------------------
Getter Method
Signature
UserPrompt()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserPrompt(userPrompt)
Parameters: userPrompt (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VarName¶
-
InspectionCmmCommandBuilder.
VarName
¶ Returns or sets the variable name
-------------------------------------
Getter Method
Signature
VarName()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VarName(varName)
Parameters: varName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VarScope¶
-
InspectionCmmCommandBuilder.
VarScope
¶ Returns or sets the variable scope
-------------------------------------
Getter Method
Signature
VarScope()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderVarScopes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VarScope(varScope)
Parameters: varScope ( NXOpen.CAM.InspectionCmmCommandBuilderVarScopes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VarType¶
-
InspectionCmmCommandBuilder.
VarType
¶ Returns or sets the variable type
-------------------------------------
Getter Method
Signature
VarType()
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderVarTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VarType(varType)
Parameters: varType ( NXOpen.CAM.InspectionCmmCommandBuilderVarTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VectorPlaces¶
-
InspectionCmmCommandBuilder.
VectorPlaces
¶ Returns or sets the vector decimal places
-------------------------------------
Getter Method
Signature
VectorPlaces()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorPlaces(vectorPlaces)
Parameters: vectorPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetProgStatements¶
-
InspectionCmmCommandBuilder.
GetProgStatements
¶ Returns the program statements
Signature
GetProgStatements()
Returns: Return type: list of str New in version NX7.0.0.
License requirements: None.
SetProgStatements¶
-
InspectionCmmCommandBuilder.
SetProgStatements
¶ Sets the program statements
Signature
SetProgStatements(progStatements)
Parameters: progStatements (list of str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionCmmCommandBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.